<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックmax 17059</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/max-17059/m-p/700006#M108721</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on imx6 solo custom board with linux yocto. now working on max 17059 fuel guage IC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;its capacity is as follows:&lt;/P&gt;&lt;P&gt;5.5V-0%&lt;BR /&gt;7.4V-50%&lt;BR /&gt;8.4V-100%&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At 8.4V it shows 100% but it shows 0% at 7V only and board will be ON &amp;nbsp;for 3 to 4 hours even after it shows 0% battery.&lt;/P&gt;&lt;P&gt;How can i solve this issue?&lt;/P&gt;&lt;P&gt;Please suggest&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Rizwan Syed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Aug 2017 11:43:19 GMT</pubDate>
    <dc:creator>rizwan_s</dc:creator>
    <dc:date>2017-08-16T11:43:19Z</dc:date>
    <item>
      <title>max 17059</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/max-17059/m-p/700006#M108721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on imx6 solo custom board with linux yocto. now working on max 17059 fuel guage IC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;its capacity is as follows:&lt;/P&gt;&lt;P&gt;5.5V-0%&lt;BR /&gt;7.4V-50%&lt;BR /&gt;8.4V-100%&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At 8.4V it shows 100% but it shows 0% at 7V only and board will be ON &amp;nbsp;for 3 to 4 hours even after it shows 0% battery.&lt;/P&gt;&lt;P&gt;How can i solve this issue?&lt;/P&gt;&lt;P&gt;Please suggest&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Rizwan Syed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2017 11:43:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/max-17059/m-p/700006#M108721</guid>
      <dc:creator>rizwan_s</dc:creator>
      <dc:date>2017-08-16T11:43:19Z</dc:date>
    </item>
    <item>
      <title>Re: max 17059</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/max-17059/m-p/700007#M108722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rizwan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check sensor ground connections and software with max 17059 evk and software&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.maximintegrated.com/en/products/power/battery-management/MAX17059.html/tb_tab2" title="https://www.maximintegrated.com/en/products/power/battery-management/MAX17059.html/tb_tab2"&gt;MAX17059 1-Cell/2-Cell Fuel Gauge with ModelGauge - Maxim&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2017 23:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/max-17059/m-p/700007#M108722</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-16T23:16:36Z</dc:date>
    </item>
  </channel>
</rss>