<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unlock RNG with cst 2.3.2? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unlock-RNG-with-cst-2-3-2/m-p/699728#M108666</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could I get confirmation please about having:&lt;/P&gt;&lt;P&gt;[Unlock]&lt;BR /&gt;Engine = CAAM&lt;BR /&gt;Features = RNG&lt;/P&gt;&lt;P&gt;in the csf file. AN4581 says that this is included by default on CST v2.3+, but I've also read that it in fact &lt;EM&gt;is&lt;/EM&gt; still needed (when wanting to use this one of the two options).&lt;/P&gt;&lt;P&gt;Just wanted to double-check please. And does it only matter if encryption is being used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Aug 2017 09:25:41 GMT</pubDate>
    <dc:creator>colinhelliwell</dc:creator>
    <dc:date>2017-08-16T09:25:41Z</dc:date>
    <item>
      <title>Unlock RNG with cst 2.3.2?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unlock-RNG-with-cst-2-3-2/m-p/699728#M108666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could I get confirmation please about having:&lt;/P&gt;&lt;P&gt;[Unlock]&lt;BR /&gt;Engine = CAAM&lt;BR /&gt;Features = RNG&lt;/P&gt;&lt;P&gt;in the csf file. AN4581 says that this is included by default on CST v2.3+, but I've also read that it in fact &lt;EM&gt;is&lt;/EM&gt; still needed (when wanting to use this one of the two options).&lt;/P&gt;&lt;P&gt;Just wanted to double-check please. And does it only matter if encryption is being used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2017 09:25:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unlock-RNG-with-cst-2-3-2/m-p/699728#M108666</guid>
      <dc:creator>colinhelliwell</dc:creator>
      <dc:date>2017-08-16T09:25:41Z</dc:date>
    </item>
    <item>
      <title>Re: Unlock RNG with cst 2.3.2?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unlock-RNG-with-cst-2-3-2/m-p/699729#M108667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;one can refer to the document as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-330622"&gt;https://community.nxp.com/docs/DOC-330622&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt; color: #000000;"&gt;&lt;SPAN lang="EN-US"&gt;it seems you should add them to the u-boot.csf&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Aug 2017 08:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unlock-RNG-with-cst-2-3-2/m-p/699729#M108667</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-08-17T08:40:01Z</dc:date>
    </item>
  </channel>
</rss>