<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6 uboot package error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-package-error/m-p/699246#M108567</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem is the dash character in PR is not legal for rpm. Modify the PR in u-boot-toradex_2016.11.bbappend can address the problem. Also, the solution could be variance, what I did is to disable the original bbappend using BBMASK and add my own on my layer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Sep 2017 17:24:11 GMT</pubDate>
    <dc:creator>jasonl</dc:creator>
    <dc:date>2017-09-12T17:24:11Z</dc:date>
    <item>
      <title>IMX6 uboot package error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-package-error/m-p/699245#M108566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to compile the Colibri IMX6 Yocto Linux project from morty branch upstream but having trouble with the u-boot-toradex 2016.11. I am trying to build the rpm package. The error message is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: u-boot-toradex-2016.11-2.7.3-gitrf0e4149 do_package_write_rpm: Function failed: BUILDSPEC (log file is located at /home/yangjiel/morty-test/build/tmp/work/colibri_imx6-poky-linux-gnueabi/u-boot-toradex/2016.11-2.7.3-gitrf0e4149/temp/log.do_package_write_rpm.21361)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/yangjiel/morty-test/build/tmp/work/colibri_imx6-poky-linux-gnueabi/u-boot-toradex/2016.11-2.7.3-gitrf0e4149/temp/log.do_package_write_rpm.21361&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing python function sstate_task_prefunc&lt;BR /&gt;| DEBUG: Python function sstate_task_prefunc finished&lt;BR /&gt;| DEBUG: Executing python function do_package_write_rpm&lt;BR /&gt;| DEBUG: Executing python function read_subpackage_metadata&lt;BR /&gt;| DEBUG: Python function read_subpackage_metadata finished&lt;BR /&gt;.......&lt;BR /&gt;NOTE: Tasks Summary: Attempted 400 tasks of which 399 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is fine while building as ipk package. I want to know is it possible to build with rpm package?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Sep 2017 19:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-package-error/m-p/699245#M108566</guid>
      <dc:creator>jasonl</dc:creator>
      <dc:date>2017-09-11T19:33:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 uboot package error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-package-error/m-p/699246#M108567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem is the dash character in PR is not legal for rpm. Modify the PR in u-boot-toradex_2016.11.bbappend can address the problem. Also, the solution could be variance, what I did is to disable the original bbappend using BBMASK and add my own on my layer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 17:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-package-error/m-p/699246#M108567</guid>
      <dc:creator>jasonl</dc:creator>
      <dc:date>2017-09-12T17:24:11Z</dc:date>
    </item>
  </channel>
</rss>