<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I2C interrupt request  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I2C-interrupt-request/m-p/698619#M108507</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;In the reference manual , table 3-1 , IRQ no 67 to 69 are for I2C devices . My question is&amp;nbsp;, in case of I2C , CPU itself is the master and generates the clock for the slave device . All I2C transactions are initated by the I2C master only , then how come slave device will give the interrupt to the CPU . Please advice.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aditya Nagal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Sep 2017 11:42:45 GMT</pubDate>
    <dc:creator>adityanagal</dc:creator>
    <dc:date>2017-09-08T11:42:45Z</dc:date>
    <item>
      <title>I2C interrupt request</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C-interrupt-request/m-p/698619#M108507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;In the reference manual , table 3-1 , IRQ no 67 to 69 are for I2C devices . My question is&amp;nbsp;, in case of I2C , CPU itself is the master and generates the clock for the slave device . All I2C transactions are initated by the I2C master only , then how come slave device will give the interrupt to the CPU . Please advice.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aditya Nagal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Sep 2017 11:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C-interrupt-request/m-p/698619#M108507</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-09-08T11:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: I2C interrupt request</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C-interrupt-request/m-p/698620#M108508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adytia&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to sect.36.7.4 I2C Status Register (I2Cx_I2SR)&amp;nbsp; i.MX6SDL RM&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf" title="http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf"&gt;http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The interrupt is set when one of the following occurs:&lt;BR /&gt;• One byte transfer is completed (the interrupt is set at the falling edge of the ninth clock).&lt;BR /&gt;• An address is received that matches its own specific address in Slave Receive mode.&lt;BR /&gt;• Arbitration is lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Sep 2017 23:21:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C-interrupt-request/m-p/698620#M108508</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-08T23:21:08Z</dc:date>
    </item>
  </channel>
</rss>