<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6 WebGL performance?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-WebGL-performance/m-p/698122#M108396</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can somebody explain me what to expect from webgl on a imx6qd board? I have compiled qtwebengine and am running a qt-application in eglfs. When I run a webgl site, it works, but not smooth. Not everything gets rendered too.&lt;/P&gt;&lt;P&gt;However, the CPU load of the qtwebengine process looks rather low (10%-20%) so I have the impression it's not running in software mode. But the performance is that bad, that I cannot imagine that this is the best it can do...&lt;/P&gt;&lt;P&gt;Anybody knows what to expect? Or how I can tweak?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Oct 2017 08:39:39 GMT</pubDate>
    <dc:creator>woutervh</dc:creator>
    <dc:date>2017-10-05T08:39:39Z</dc:date>
    <item>
      <title>imx6 WebGL performance?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-WebGL-performance/m-p/698122#M108396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can somebody explain me what to expect from webgl on a imx6qd board? I have compiled qtwebengine and am running a qt-application in eglfs. When I run a webgl site, it works, but not smooth. Not everything gets rendered too.&lt;/P&gt;&lt;P&gt;However, the CPU load of the qtwebengine process looks rather low (10%-20%) so I have the impression it's not running in software mode. But the performance is that bad, that I cannot imagine that this is the best it can do...&lt;/P&gt;&lt;P&gt;Anybody knows what to expect? Or how I can tweak?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Oct 2017 08:39:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-WebGL-performance/m-p/698122#M108396</guid>
      <dc:creator>woutervh</dc:creator>
      <dc:date>2017-10-05T08:39:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 WebGL performance?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-WebGL-performance/m-p/698123#M108397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have same issue, my customers complain for their HTML5 game is very no smooth, we use Chrome on Android 7.1 using imx6Q platform, CPU looks only spend 50% usage, vmalloc=512M, it's not make sense running without smooth, how to improve?&lt;BR /&gt;&lt;BR /&gt;Resolution: 720P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Nov 2017 15:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-WebGL-performance/m-p/698123#M108397</guid>
      <dc:creator>mayqueen</dc:creator>
      <dc:date>2017-11-17T15:30:27Z</dc:date>
    </item>
  </channel>
</rss>