<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Building u-boot for imx6 solo in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698050#M108384</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Durgesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was asking for the u-boot version, not the defconfig. Let me explain:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you build a NXP's BSP for i.MX using the command 'bitbake' you will get a .sdcard file which contains the uboot, the kernel (zImage), the device tree (.dtb) and the root file system. In this case you dont need the defconfig because everything is set on recipes. You can deploy the full image with command 'dd' using the .sdcard file.&lt;/P&gt;&lt;P&gt;In my opinion this is your best option. You can also deploy zImage or uboot or root file system separately. In the following post you will find details about this: &lt;A href="https://community.nxp.com/docs/DOC-94989"&gt;Task #4 - Deploy and test&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Besides this, you can extract the source out of Yocto, in this case you can make using imx_v7_defconfig.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand you can clone u-boot from community &lt;A class="link-titled" href="https://github.com/Freescale/u-boot-fslc/tree/2016.11+fslc" title="https://github.com/Freescale/u-boot-fslc/tree/2016.11+fslc"&gt;GitHub - Freescale/u-boot-fslc at 2016.11+fslc&lt;/A&gt;&amp;nbsp; and you can build it using mx6dlsabresd_defconfig. Please note that this is a community external to NXP so this u-boot is not supported by NXP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that the defconfig files are specific for boards, not for MCUs, therefore if you are using a custom board the defconfig may not work for you as you may need to customize it to match your board.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Sep 2017 16:49:15 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2017-09-12T16:49:15Z</dc:date>
    <item>
      <title>Building u-boot for imx6 solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698044#M108378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a new CPU module with iMX6 Solo and 512 MB RAM. Can you tell me which config to use to compile u-boot source? I dint see any config which can be used for SOLO. i tried nitrogen6s_defconfig and u-boot can boot but obviously lots of errors as my module is not nitrogen.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Sep 2017 04:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698044#M108378</guid>
      <dc:creator>d_saxena</dc:creator>
      <dc:date>2017-09-08T04:08:36Z</dc:date>
    </item>
    <item>
      <title>Re: Building u-boot for imx6 solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698045#M108379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dargesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP does not provide support for Nitrogen boards, but probably &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/gary_bisson"&gt;gary_bisson&lt;/A&gt;‌ may comment on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Sep 2017 16:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698045#M108379</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-09-08T16:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: Building u-boot for imx6 solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698046#M108380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My understanding is that the module is NOT a Nitrogen one so I can't help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dargesh, please specify the exact reference of the module you are using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Sep 2017 16:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698046#M108380</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2017-09-08T16:33:00Z</dc:date>
    </item>
    <item>
      <title>Re: Building u-boot for imx6 solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698047#M108381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Our design is based on SabreSD board. First CPU module has iMX6 quad core and 2 GB RAM. I made u-boot and linux image for that. No issues in that area.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now the hardware designer has replaces CPU with iMX6 SOLO and reduced memory to 512 in new board. According to hardware designer SOLO and quad is pin to pin compatible and interchangeable. Now i have following configuration...&lt;/P&gt;&lt;P&gt;CPU iMX6 SOLO&lt;/P&gt;&lt;P&gt;RAM 512 MB&lt;/P&gt;&lt;P&gt;base board design reference is SabreSD...&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Sep 2017 06:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698047#M108381</guid>
      <dc:creator>d_saxena</dc:creator>
      <dc:date>2017-09-09T06:46:19Z</dc:date>
    </item>
    <item>
      <title>Re: Building u-boot for imx6 solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698048#M108382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Durgesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which u-boot are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Sep 2017 17:26:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698048#M108382</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-09-11T17:26:25Z</dc:date>
    </item>
    <item>
      <title>Re: Building u-boot for imx6 solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698049#M108383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;That was my question... I did not find defconfig for SOLO.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 01:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698049#M108383</guid>
      <dc:creator>d_saxena</dc:creator>
      <dc:date>2017-09-12T01:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: Building u-boot for imx6 solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698050#M108384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Durgesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was asking for the u-boot version, not the defconfig. Let me explain:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you build a NXP's BSP for i.MX using the command 'bitbake' you will get a .sdcard file which contains the uboot, the kernel (zImage), the device tree (.dtb) and the root file system. In this case you dont need the defconfig because everything is set on recipes. You can deploy the full image with command 'dd' using the .sdcard file.&lt;/P&gt;&lt;P&gt;In my opinion this is your best option. You can also deploy zImage or uboot or root file system separately. In the following post you will find details about this: &lt;A href="https://community.nxp.com/docs/DOC-94989"&gt;Task #4 - Deploy and test&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Besides this, you can extract the source out of Yocto, in this case you can make using imx_v7_defconfig.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand you can clone u-boot from community &lt;A class="link-titled" href="https://github.com/Freescale/u-boot-fslc/tree/2016.11+fslc" title="https://github.com/Freescale/u-boot-fslc/tree/2016.11+fslc"&gt;GitHub - Freescale/u-boot-fslc at 2016.11+fslc&lt;/A&gt;&amp;nbsp; and you can build it using mx6dlsabresd_defconfig. Please note that this is a community external to NXP so this u-boot is not supported by NXP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that the defconfig files are specific for boards, not for MCUs, therefore if you are using a custom board the defconfig may not work for you as you may need to customize it to match your board.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 16:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Building-u-boot-for-imx6-solo/m-p/698050#M108384</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-09-12T16:49:15Z</dc:date>
    </item>
  </channel>
</rss>