<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Host Controller Interface issue in IMX53 QSB android 2.3.4</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199384#M10837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I downloaded gingerbread android 2.3.4 and 2.6.35.3 kernel. I have built that android version for IMX53 QSB and I'm using a SDIO supported WIFI card in the SDIO slot provided in IMX53 QSB. I have a problem in sending data down to the device. The packet for which I issue a cmd53 write (packet size: 256) has some non-zero bytes in it. However, when the packet reaches the device, the data somehow gets corrupted and I get to see zeroes instead of valid data.&lt;/P&gt;&lt;P&gt;Can anyone please help in resolving this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Swaraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Jan 2012 12:15:36 GMT</pubDate>
    <dc:creator>swaraj</dc:creator>
    <dc:date>2012-01-02T12:15:36Z</dc:date>
    <item>
      <title>Host Controller Interface issue in IMX53 QSB android 2.3.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199384#M10837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I downloaded gingerbread android 2.3.4 and 2.6.35.3 kernel. I have built that android version for IMX53 QSB and I'm using a SDIO supported WIFI card in the SDIO slot provided in IMX53 QSB. I have a problem in sending data down to the device. The packet for which I issue a cmd53 write (packet size: 256) has some non-zero bytes in it. However, when the packet reaches the device, the data somehow gets corrupted and I get to see zeroes instead of valid data.&lt;/P&gt;&lt;P&gt;Can anyone please help in resolving this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Swaraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jan 2012 12:15:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199384#M10837</guid>
      <dc:creator>swaraj</dc:creator>
      <dc:date>2012-01-02T12:15:36Z</dc:date>
    </item>
  </channel>
</rss>