<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 Android UVC (USB Video Class) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-UVC-USB-Video-Class/m-p/697295#M108257</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Customer has developed the system with android jb4.2.2_1.1.0-ga(from Freescale/NXP) on IMX6DualLite.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;It can use the USB camera of UVC by using Android standard Camera API.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Q.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is the following module related to UVC operation?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/device/fsl-proprietary/gpu-viv/lib/libg2d.so&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Eishi SHIBUSAWA&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Oct 2017 00:49:25 GMT</pubDate>
    <dc:creator>eishishibusawa</dc:creator>
    <dc:date>2017-10-04T00:49:25Z</dc:date>
    <item>
      <title>i.MX6 Android UVC (USB Video Class)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-UVC-USB-Video-Class/m-p/697295#M108257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Customer has developed the system with android jb4.2.2_1.1.0-ga(from Freescale/NXP) on IMX6DualLite.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;It can use the USB camera of UVC by using Android standard Camera API.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Q.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is the following module related to UVC operation?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/device/fsl-proprietary/gpu-viv/lib/libg2d.so&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Eishi SHIBUSAWA&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Oct 2017 00:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-UVC-USB-Video-Class/m-p/697295#M108257</guid>
      <dc:creator>eishishibusawa</dc:creator>
      <dc:date>2017-10-04T00:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Android UVC (USB Video Class)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-UVC-USB-Video-Class/m-p/697296#M108258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eishi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this file has not direct relation to usb module operations, just for&lt;/P&gt;&lt;P&gt;reference please refer to sect.11.1.1.3 Source Code Structure&lt;/P&gt;&lt;P&gt;attached Linux Manual for L3.0.35 which is used in &lt;SPAN&gt;android jb4.2.2&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Oct 2017 05:46:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Android-UVC-USB-Video-Class/m-p/697296#M108258</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-10-04T05:46:14Z</dc:date>
    </item>
  </channel>
</rss>