<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Host Controller Interface issue in IMX53 QSB android 2.3.4 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199114#M10807</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Remi Lorriaux,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;It is a redpine chip. The redpine wifi card is working fine with other boards like IMX28, IMX51, IMX53 linux .&lt;/P&gt;&lt;P&gt;But it is not working for android IMX53 QSB. When i debugged, i found there is something wrong in host controller while sending data packets.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jan 2012 04:13:21 GMT</pubDate>
    <dc:creator>swaraj</dc:creator>
    <dc:date>2012-01-04T04:13:21Z</dc:date>
    <item>
      <title>Host Controller Interface issue in IMX53 QSB android 2.3.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199112#M10805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I downloaded gingerbread android 2.3.4 and 2.6.35.3 kernel. I have built that android version for IMX53 QSB and I'm using a SDIO supported WIFI card in the SDIO slot provided in IMX53 QSB. I have a problem in sending data down to the device. The packet for which I issue a cmd53 write (packet size: 256) has some non-zero bytes in it. However, when the packet reaches the device, the data somehow gets corrupted and I get to see zeroes instead of valid data.&lt;/P&gt;&lt;P&gt;Can anyone please help in resolving this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt; Swaraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jan 2012 12:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199112#M10805</guid>
      <dc:creator>swaraj</dc:creator>
      <dc:date>2012-01-02T12:16:45Z</dc:date>
    </item>
    <item>
      <title>Re: Host Controller Interface issue in IMX53 QSB android 2.3.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199113#M10806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Which Wifi device are you using? Is it one of the Atheros chips?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2012 23:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199113#M10806</guid>
      <dc:creator>rlorriaux</dc:creator>
      <dc:date>2012-01-03T23:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: Host Controller Interface issue in IMX53 QSB android 2.3.4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199114#M10807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Remi Lorriaux,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;It is a redpine chip. The redpine wifi card is working fine with other boards like IMX28, IMX51, IMX53 linux .&lt;/P&gt;&lt;P&gt;But it is not working for android IMX53 QSB. When i debugged, i found there is something wrong in host controller while sending data packets.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2012 04:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Host-Controller-Interface-issue-in-IMX53-QSB-android-2-3-4/m-p/199114#M10807</guid>
      <dc:creator>swaraj</dc:creator>
      <dc:date>2012-01-04T04:13:21Z</dc:date>
    </item>
  </channel>
</rss>