<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX7D Qspi change clock issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Qspi-change-clock-issue/m-p/696009#M108011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used a serial flash on IMX7D target board, when the spi clcok is 29M, It works well, but when I change it to 84M,&lt;/P&gt;&lt;P&gt;read data error,IF I write data at 84M and read it at 29M, it is ok. But if 84M write data and 84M read data, It faild.&lt;/P&gt;&lt;P&gt;So ,if I change the spi clock frequence, what&amp;nbsp; othre parameters should I change at the same time for the quadspi controller?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Aug 2017 06:30:55 GMT</pubDate>
    <dc:creator>xujibin</dc:creator>
    <dc:date>2017-08-10T06:30:55Z</dc:date>
    <item>
      <title>IMX7D Qspi change clock issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Qspi-change-clock-issue/m-p/696009#M108011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used a serial flash on IMX7D target board, when the spi clcok is 29M, It works well, but when I change it to 84M,&lt;/P&gt;&lt;P&gt;read data error,IF I write data at 84M and read it at 29M, it is ok. But if 84M write data and 84M read data, It faild.&lt;/P&gt;&lt;P&gt;So ,if I change the spi clock frequence, what&amp;nbsp; othre parameters should I change at the same time for the quadspi controller?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2017 06:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Qspi-change-clock-issue/m-p/696009#M108011</guid>
      <dc:creator>xujibin</dc:creator>
      <dc:date>2017-08-10T06:30:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D Qspi change clock issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Qspi-change-clock-issue/m-p/696010#M108012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;About the i.MX7D qspi clock setting you can refer to the reference manual IMX7DRM.pdf.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="QSPI CLOCK.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30125iBB5F54C3BB9A58F7/image-size/large?v=v2&amp;amp;px=999" role="button" title="QSPI CLOCK.PNG" alt="QSPI CLOCK.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Sep 2017 08:30:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Qspi-change-clock-issue/m-p/696010#M108012</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-09-14T08:30:21Z</dc:date>
    </item>
  </channel>
</rss>