<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestion about OCRAM_PXP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-OCRAM-PXP/m-p/695283#M107808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;question about OCRAM_PXP.&lt;/P&gt;&lt;P&gt;I can't understand which memory use in default in each case&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1.&lt;/P&gt;&lt;P&gt;Is OCRAM_PXP always used when PXP (rotation, superimposition, CSC) is used ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2.&lt;/P&gt;&lt;P&gt;My recognition is that PXP is not used when outputting from LCDIF to LCD through the camera.&lt;BR /&gt;In this case, is it&amp;nbsp;correct&amp;nbsp; that OCRAM_PXP is not used ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ko-hey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Sep 2017 09:07:52 GMT</pubDate>
    <dc:creator>ko-hey</dc:creator>
    <dc:date>2017-09-06T09:07:52Z</dc:date>
    <item>
      <title>Question about OCRAM_PXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-OCRAM-PXP/m-p/695283#M107808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;question about OCRAM_PXP.&lt;/P&gt;&lt;P&gt;I can't understand which memory use in default in each case&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1.&lt;/P&gt;&lt;P&gt;Is OCRAM_PXP always used when PXP (rotation, superimposition, CSC) is used ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2.&lt;/P&gt;&lt;P&gt;My recognition is that PXP is not used when outputting from LCDIF to LCD through the camera.&lt;BR /&gt;In this case, is it&amp;nbsp;correct&amp;nbsp; that OCRAM_PXP is not used ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ko-hey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 09:07:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-OCRAM-PXP/m-p/695283#M107808</guid>
      <dc:creator>ko-hey</dc:creator>
      <dc:date>2017-09-06T09:07:52Z</dc:date>
    </item>
    <item>
      <title>Re: Question about OCRAM_PXP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-about-OCRAM-PXP/m-p/695284#M107809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; OCRAM_PXP mainly is used, when&amp;nbsp; the PXP and LCDIF support a mode where&lt;/P&gt;&lt;P&gt;the internal RAM serves as&amp;nbsp; frame buffer to minimize external memory bandwidth.&lt;/P&gt;&lt;P&gt;Also, You may look at Figure 13-87 (PXP Architecture) of i.MX7D RM, showing&amp;nbsp;Internal&lt;BR /&gt;RAM using. So, it is not recommended to use OCRAM_PXP, when the PXP is working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; It is possible to implement data path from CSI camera to LCD without PXP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Also, please look at &lt;A href="https://community.nxp.com/thread/451359"&gt;About OCRAM_S in i.MX7Solo&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2017 07:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-about-OCRAM-PXP/m-p/695284#M107809</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-09-07T07:57:29Z</dc:date>
    </item>
  </channel>
</rss>