<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX7/PF3000 RTC Backup Power in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PF3000-RTC-Backup-Power/m-p/695121#M107752</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering about the RTC section of the i.MX7 and power supply in combination with a PF3000 PMIC and if I understood everything correctly.&lt;BR /&gt;Based on this I want to decide wether the i.MX7 internal RTC is suited or if an external RTC is the way to go.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PF3000 / i.MX7 provide NVCC voltage rails for e.g. the RTC. These allow power states&amp;nbsp;with most of the system disabled, including many power rails, clocks, cores etc.&amp;nbsp;If the systems power is cut&amp;nbsp;the NVCC voltage rails should not be powered anymore. Some kind of backup power supply for the RTC is needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On pin 36 (LICELL) a Lithium Cell may be connected to the system. The PF3000 provides an internal LiCell charger. Registers allow to enable/disable the charger and to set the batterys/caps voltage. All SNVS regions are powered by either an internal LDO (if the systems input voltage is above a certain threshold) or the battery.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Coin cell power mode (all power rails etc turned off) current consumption: up to 7uA based on '5.3 - current consumption' in the PF3000 datasheet. This is probably the current consumption of the PF3000 itsself?&lt;BR /&gt;It is said the current will increase when the voltage drops, up to 50uA. Are there any graphs or additional info on how the current increases?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot find information on the i.MX7D current consumption when only the SNVS rails are powered. Only information I&amp;nbsp;could find is&amp;nbsp;in another thread:&amp;nbsp;&lt;A class="link-titled" href="https://nxpcommunity.force.com/s/question/0D55700005OHnMFCA1/imx7-snvs-power-consumption" title="https://nxpcommunity.force.com/s/question/0D55700005OHnMFCA1/imx7-snvs-power-consumption"&gt;NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on this, around 500uA at 3V are&amp;nbsp;consume. For a 4 Month backup (from PCB manufacturing until system delivery),&amp;nbsp;assuming constant voltage and current, a 1.4 Ah battery is necessary, (without self discharge) (correct?).&lt;BR /&gt;As an alternative, a supercap storing 1.4Ah*3V = 4,2 Wh = 15 kWs could be used. For a voltage drop of 2V7 .. 1V8, this means a 7500F capacitor (!!!) is required, so a capacitor is out of question. Or did I&amp;nbsp;miscalculate here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dedicated RTCs require about 50nA supply current, what is just 1/10000 of the mx7 requirement. I should certainly go with a dedicated RTC, if the assumptions above are correct and if the mx7 + pf3000 RTC power backup really consumes about 500uA continously when powered off.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Sep 2017 12:27:55 GMT</pubDate>
    <dc:creator>demoniacmilk</dc:creator>
    <dc:date>2017-09-06T12:27:55Z</dc:date>
    <item>
      <title>i.MX7/PF3000 RTC Backup Power</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PF3000-RTC-Backup-Power/m-p/695121#M107752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering about the RTC section of the i.MX7 and power supply in combination with a PF3000 PMIC and if I understood everything correctly.&lt;BR /&gt;Based on this I want to decide wether the i.MX7 internal RTC is suited or if an external RTC is the way to go.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PF3000 / i.MX7 provide NVCC voltage rails for e.g. the RTC. These allow power states&amp;nbsp;with most of the system disabled, including many power rails, clocks, cores etc.&amp;nbsp;If the systems power is cut&amp;nbsp;the NVCC voltage rails should not be powered anymore. Some kind of backup power supply for the RTC is needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On pin 36 (LICELL) a Lithium Cell may be connected to the system. The PF3000 provides an internal LiCell charger. Registers allow to enable/disable the charger and to set the batterys/caps voltage. All SNVS regions are powered by either an internal LDO (if the systems input voltage is above a certain threshold) or the battery.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Coin cell power mode (all power rails etc turned off) current consumption: up to 7uA based on '5.3 - current consumption' in the PF3000 datasheet. This is probably the current consumption of the PF3000 itsself?&lt;BR /&gt;It is said the current will increase when the voltage drops, up to 50uA. Are there any graphs or additional info on how the current increases?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot find information on the i.MX7D current consumption when only the SNVS rails are powered. Only information I&amp;nbsp;could find is&amp;nbsp;in another thread:&amp;nbsp;&lt;A class="link-titled" href="https://nxpcommunity.force.com/s/question/0D55700005OHnMFCA1/imx7-snvs-power-consumption" title="https://nxpcommunity.force.com/s/question/0D55700005OHnMFCA1/imx7-snvs-power-consumption"&gt;NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on this, around 500uA at 3V are&amp;nbsp;consume. For a 4 Month backup (from PCB manufacturing until system delivery),&amp;nbsp;assuming constant voltage and current, a 1.4 Ah battery is necessary, (without self discharge) (correct?).&lt;BR /&gt;As an alternative, a supercap storing 1.4Ah*3V = 4,2 Wh = 15 kWs could be used. For a voltage drop of 2V7 .. 1V8, this means a 7500F capacitor (!!!) is required, so a capacitor is out of question. Or did I&amp;nbsp;miscalculate here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dedicated RTCs require about 50nA supply current, what is just 1/10000 of the mx7 requirement. I should certainly go with a dedicated RTC, if the assumptions above are correct and if the mx7 + pf3000 RTC power backup really consumes about 500uA continously when powered off.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 12:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PF3000-RTC-Backup-Power/m-p/695121#M107752</guid>
      <dc:creator>demoniacmilk</dc:creator>
      <dc:date>2017-09-06T12:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7/PF3000 RTC Backup Power</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PF3000-RTC-Backup-Power/m-p/695122#M107753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; In general Your considerations are correct. Note, according to &amp;nbsp;i.MX7D Datasheet :&lt;BR /&gt;SNVS mode is also called RTC mode, where only the power for the SNVS domain remain on.&lt;/P&gt;&lt;P&gt;In this mode, only the RTC and tamper detection logic is still active. The power consumption in SNVS&lt;/P&gt;&lt;P&gt;mode with all the tamper detection logic enabled will be less than 5 uA @ 3.0 V on VDD_SNVS_IN for typical&lt;/P&gt;&lt;P&gt;silicon at 25°C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; External RTC may be preferable solution when it is needed to get coin cell based power during&lt;/P&gt;&lt;P&gt;long time. It is very hard to create RTC with nA consumption as part of a SOC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2017 09:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PF3000-RTC-Backup-Power/m-p/695122#M107753</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-09-07T09:03:21Z</dc:date>
    </item>
  </channel>
</rss>