<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eglSwapBuffers Behaviour X11 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eglSwapBuffers-Behaviour-X11/m-p/694990#M107733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to understand the behavior of eglSwapBuffers().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was under the impression that if my rendering code took 4ms, eglSwapBuffers will block the thread for 16.7ms - 4ms.&lt;/P&gt;&lt;P&gt;However, when I tried measuring the time taken between eglSwapBuffers, the time is 4ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this due to X11? Will be trying DirectFB for comparison.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in the mean time, would appreciate it if anyone can enlighten me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the i.MX6QP-SABRE-SD with Linux 4.1.15_2.0.1 Patch.&lt;/P&gt;&lt;P&gt;My output is &lt;A href="mailto:800x600@60Hz on"&gt;800x600@60Hz on&lt;/A&gt; HDMI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jacob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Sep 2017 06:47:58 GMT</pubDate>
    <dc:creator>jacoblim</dc:creator>
    <dc:date>2017-09-06T06:47:58Z</dc:date>
    <item>
      <title>eglSwapBuffers Behaviour X11</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eglSwapBuffers-Behaviour-X11/m-p/694990#M107733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to understand the behavior of eglSwapBuffers().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was under the impression that if my rendering code took 4ms, eglSwapBuffers will block the thread for 16.7ms - 4ms.&lt;/P&gt;&lt;P&gt;However, when I tried measuring the time taken between eglSwapBuffers, the time is 4ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this due to X11? Will be trying DirectFB for comparison.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in the mean time, would appreciate it if anyone can enlighten me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the i.MX6QP-SABRE-SD with Linux 4.1.15_2.0.1 Patch.&lt;/P&gt;&lt;P&gt;My output is &lt;A href="mailto:800x600@60Hz on"&gt;800x600@60Hz on&lt;/A&gt; HDMI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jacob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 06:47:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eglSwapBuffers-Behaviour-X11/m-p/694990#M107733</guid>
      <dc:creator>jacoblim</dc:creator>
      <dc:date>2017-09-06T06:47:58Z</dc:date>
    </item>
    <item>
      <title>Re: eglSwapBuffers Behaviour X11</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eglSwapBuffers-Behaviour-X11/m-p/694991#M107734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jacob,&lt;/P&gt;&lt;P&gt;You could take a look at the following thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/564472"&gt;https://community.nxp.com/message/564472&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 16:34:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eglSwapBuffers-Behaviour-X11/m-p/694991#M107734</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2017-09-18T16:34:23Z</dc:date>
    </item>
  </channel>
</rss>