<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 1.8V simulation of RGMII interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/1-8V-simulation-of-RGMII-interface/m-p/694457#M107664</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to do SI simulation on teh RGMII Interface and use the current i.MX6Q IBIS model together with the appropriate IBIS model of the connected PHY.&lt;/P&gt;&lt;P&gt;The PHA as well as the i.MX6 can operate in 1.8V, 2.5V and 3.3V signbaling - but the IBIS model of teh i.MX6 has only 2.5V Output Driver models&lt;/P&gt;&lt;P&gt;Are there any intentions to add those lower voltages to teh model or do I Need to model with 2.5 and assume, that the results will be similar with 1.8V signaling?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Aug 2017 06:45:27 GMT</pubDate>
    <dc:creator>inmaku</dc:creator>
    <dc:date>2017-08-09T06:45:27Z</dc:date>
    <item>
      <title>1.8V simulation of RGMII interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/1-8V-simulation-of-RGMII-interface/m-p/694457#M107664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to do SI simulation on teh RGMII Interface and use the current i.MX6Q IBIS model together with the appropriate IBIS model of the connected PHY.&lt;/P&gt;&lt;P&gt;The PHA as well as the i.MX6 can operate in 1.8V, 2.5V and 3.3V signbaling - but the IBIS model of teh i.MX6 has only 2.5V Output Driver models&lt;/P&gt;&lt;P&gt;Are there any intentions to add those lower voltages to teh model or do I Need to model with 2.5 and assume, that the results will be similar with 1.8V signaling?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 06:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/1-8V-simulation-of-RGMII-interface/m-p/694457#M107664</guid>
      <dc:creator>inmaku</dc:creator>
      <dc:date>2017-08-09T06:45:27Z</dc:date>
    </item>
    <item>
      <title>Re: 1.8V simulation of RGMII interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/1-8V-simulation-of-RGMII-interface/m-p/694458#M107665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="213582" data-username="inmaku" href="https://community.nxp.com/people/inmaku"&gt;Ingo&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; It is no problem for you to use 2.5V to do simulation. Result is not affected by voltage of RGMII.&amp;nbsp; Several days ago, a customer used a 1.8V-PHY manufactured by Realtek, and no any problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 07:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/1-8V-simulation-of-RGMII-interface/m-p/694458#M107665</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-08-09T07:21:07Z</dc:date>
    </item>
  </channel>
</rss>