<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  Load current of GPIO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Load-current-of-GPIO/m-p/694140#M107625</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually GPIO buffer load capacity is not specified in units of current.&lt;BR /&gt;It is only specified in terms of buffer drive strength or output impedance.&lt;BR /&gt;You can refer chapter 4.8.1 "Single Voltage GPIO Output Buffer Impedance" of i.MX 6UltraLite DataSheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you can use IBIS models to estimate the current.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day, &lt;BR /&gt;Victor &lt;BR /&gt; &lt;BR /&gt;----------------------------------------------------------------------------------------------------------------------- &lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you! &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Aug 2017 06:57:00 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-08-09T06:57:00Z</dc:date>
    <item>
      <title>Load current of GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Load-current-of-GPIO/m-p/694139#M107624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using i.Mx6UL based custom board. &lt;BR /&gt; We need withstand load current of GPIO pin for appropriate LED selection(Considering GPIO voltage as 3.3V).&lt;BR /&gt;I could not find this detail in the datasheet. Please provide the detail on this.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Krishna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 01:27:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Load-current-of-GPIO/m-p/694139#M107624</guid>
      <dc:creator>KrishnaPrasad1z</dc:creator>
      <dc:date>2017-08-09T01:27:44Z</dc:date>
    </item>
    <item>
      <title>Re:  Load current of GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Load-current-of-GPIO/m-p/694140#M107625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually GPIO buffer load capacity is not specified in units of current.&lt;BR /&gt;It is only specified in terms of buffer drive strength or output impedance.&lt;BR /&gt;You can refer chapter 4.8.1 "Single Voltage GPIO Output Buffer Impedance" of i.MX 6UltraLite DataSheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you can use IBIS models to estimate the current.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day, &lt;BR /&gt;Victor &lt;BR /&gt; &lt;BR /&gt;----------------------------------------------------------------------------------------------------------------------- &lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you! &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 06:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Load-current-of-GPIO/m-p/694140#M107625</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-08-09T06:57:00Z</dc:date>
    </item>
  </channel>
</rss>