<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Pins for IMX Tool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pins-for-IMX-Tool/m-p/693294#M107505</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gopinath Srinivasan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The included help topics are indeed very helpful so I would recommend reviewing this information as there is no further documentation (other than the installation guide).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code generated can be used by u-boot to load the appropriate register values and the dtsi file has the information that has to be added to the device tree in order to configure the pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the sabre board file you mean the Pin configuration file for the SABRE board? When you select File&amp;gt;New you can find some boards and load the muxing configuration for these boards, which is helpful if you based your design on one of these boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 May 2017 20:32:32 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-05-26T20:32:32Z</dc:date>
    <item>
      <title>Pins for IMX Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pins-for-IMX-Tool/m-p/693292#M107503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am working on porting custom IMX7 processor based on Sabresd board. I have downloaded Pins for IMX tool for Linux-ubuntu. &amp;nbsp;I tried to export my IMX7 project using pin mux tool as source file and I got the below files as output.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;pin_mux.h,&amp;nbsp;pin_mux.c,&amp;nbsp;iMX7D_registers.h,imx7d-board.dtsi,fsl_bitaccess.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have below questions,&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Is it possible to generate u-boot pixmux file using this tool?&lt;/P&gt;&lt;P&gt;2.How can I import the sabresd pin mux file (I mean which file I need give as import) so that I can do the customisation of my board pin configuration easily?&lt;/P&gt;&lt;P&gt;3. Can I get any documents for this pin mux tools?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 May 2017 13:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pins-for-IMX-Tool/m-p/693292#M107503</guid>
      <dc:creator>gopinathsriniva</dc:creator>
      <dc:date>2017-05-25T13:45:22Z</dc:date>
    </item>
    <item>
      <title>Re: Pins for IMX Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pins-for-IMX-Tool/m-p/693293#M107504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please run the tool and go to the Help -&amp;gt; Contents menu. It describes all required procedures in details.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 07:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pins-for-IMX-Tool/m-p/693293#M107504</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-05-26T07:27:04Z</dc:date>
    </item>
    <item>
      <title>Re: Pins for IMX Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pins-for-IMX-Tool/m-p/693294#M107505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gopinath Srinivasan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The included help topics are indeed very helpful so I would recommend reviewing this information as there is no further documentation (other than the installation guide).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code generated can be used by u-boot to load the appropriate register values and the dtsi file has the information that has to be added to the device tree in order to configure the pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the sabre board file you mean the Pin configuration file for the SABRE board? When you select File&amp;gt;New you can find some boards and load the muxing configuration for these boards, which is helpful if you based your design on one of these boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 20:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pins-for-IMX-Tool/m-p/693294#M107505</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-05-26T20:32:32Z</dc:date>
    </item>
  </channel>
</rss>