<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: BitInit source request - to work on x64</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691575#M107150</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have searched for you, but do not found the source code you need. I will do further confirm for you.&lt;/P&gt;&lt;P&gt;Here you can try to use the MFG Tool to set the OTP Bits. The MFG Tool also has some flaws in 64bit environments (when clicking on Options-&amp;gt;Configurations-&amp;gt;USBport the program crashes, so just don't click there), but it works well enough to burn the OTP bits.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Aug 2017 08:07:21 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2017-08-09T08:07:21Z</dc:date>
    <item>
      <title>BitInit source request - to work on x64</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691572#M107147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems there are a few documented cases of BitInit not working on Windows 64 bit platforms. &amp;nbsp;Can NXP please provide the source for BitInit so that I can recompile and fix the issues? &amp;nbsp;I understand that I might be able to get MFGTool to work but it would be much easier to call BitInit from the command line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BitInit.exe (Version 2.2.3796.13940)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;System.ComponentModel.Win32Exception: The supplied user buffer is not valid for the requested operation&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 20:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691572#M107147</guid>
      <dc:creator>andrewsedlmayr</dc:creator>
      <dc:date>2017-08-02T20:33:11Z</dc:date>
    </item>
    <item>
      <title>Re: BitInit source request - to work on x64</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691573#M107148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In our website all the code and tools are here &lt;A class="link-titled" href="http://www.nxp.com/products/developer-resources/software-development-tools/i.mx-software-and-tools/i.mx28-evaluation-kit:MCIMX28EVKJ?tab=Design_Tools_Tab" title="http://www.nxp.com/products/developer-resources/software-development-tools/i.mx-software-and-tools/i.mx28-evaluation-kit:MCIMX28EVKJ?tab=Design_Tools_Tab"&gt;i.MX28 Evaluation Kit|NXP&lt;/A&gt; . And the default Bitlnit work on windows PC 32bit. Here&amp;nbsp; I found one thread follow, hope it can do help for you.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/311653"&gt;BitInit Exception "user buffer is not valid"&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/docs/en/application-note/AN4555.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://cache.nxp.com/docs/en/application-note/AN4555.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;http://cache.nxp.com/docs/en/application-note/AN4555.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&lt;/A&gt; &lt;BR /&gt;Have a great day,&lt;BR /&gt; Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 08:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691573#M107148</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-08-03T08:19:05Z</dc:date>
    </item>
    <item>
      <title>Re: BitInit source request - to work on x64</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691574#M107149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am requesting the SOURCE code so I can recompile for 64 bit machines. &amp;nbsp;I do not see the source code available anywhere. &amp;nbsp;If you cannot provide the source, please provide an executable that works on 64 bit platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 14:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691574#M107149</guid>
      <dc:creator>andrewsedlmayr</dc:creator>
      <dc:date>2017-08-03T14:03:31Z</dc:date>
    </item>
    <item>
      <title>Re: BitInit source request - to work on x64</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691575#M107150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have searched for you, but do not found the source code you need. I will do further confirm for you.&lt;/P&gt;&lt;P&gt;Here you can try to use the MFG Tool to set the OTP Bits. The MFG Tool also has some flaws in 64bit environments (when clicking on Options-&amp;gt;Configurations-&amp;gt;USBport the program crashes, so just don't click there), but it works well enough to burn the OTP bits.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 08:07:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitInit-source-request-to-work-on-x64/m-p/691575#M107150</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-08-09T08:07:21Z</dc:date>
    </item>
  </channel>
</rss>