<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic linux kernel is halt when open the ipu_channel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/linux-kernel-is-halt-when-open-the-ipu-channel/m-p/689749#M106828</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi~&lt;BR /&gt; I having a very ticklish question, I open the ipu channel through calli the ipuv3 driver(through the function static int capture_open(struct inode *inode, struct file *file)), the linux kernel is halt without any trace log, show the message:&lt;BR /&gt;enter ipu_err_irq_handler.IRQ:37&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001&lt;BR /&gt;later the kernel is halt, I have to power off and power on to restart the system.I can't understand the problem, please help me. thank you very much!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ps:my kernel is linux 3.14.52&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336496"&gt;ipu-csi-capture.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Jun 2017 03:52:37 GMT</pubDate>
    <dc:creator>wwfdzh2012</dc:creator>
    <dc:date>2017-06-17T03:52:37Z</dc:date>
    <item>
      <title>linux kernel is halt when open the ipu_channel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-kernel-is-halt-when-open-the-ipu-channel/m-p/689749#M106828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi~&lt;BR /&gt; I having a very ticklish question, I open the ipu channel through calli the ipuv3 driver(through the function static int capture_open(struct inode *inode, struct file *file)), the linux kernel is halt without any trace log, show the message:&lt;BR /&gt;enter ipu_err_irq_handler.IRQ:37&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001&lt;BR /&gt;later the kernel is halt, I have to power off and power on to restart the system.I can't understand the problem, please help me. thank you very much!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ps:my kernel is linux 3.14.52&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336496"&gt;ipu-csi-capture.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Jun 2017 03:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-kernel-is-halt-when-open-the-ipu-channel/m-p/689749#M106828</guid>
      <dc:creator>wwfdzh2012</dc:creator>
      <dc:date>2017-06-17T03:52:37Z</dc:date>
    </item>
    <item>
      <title>Re: linux kernel is halt when open the ipu_channel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-kernel-is-halt-when-open-the-ipu-channel/m-p/689750#M106829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check that ipu clock is not gated on CCM_CCGR3&lt;/P&gt;&lt;P&gt;register. Also may be useful to check if this is not hardware problem:&lt;/P&gt;&lt;P&gt;run ddr test and check processor power supplies. Please follow guidelines in&lt;/P&gt;&lt;P&gt;i.MX6 System Development User’s Guide&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fuser_guide%2FIMX6DQ6SDLHDG.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Jun 2017 23:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-kernel-is-halt-when-open-the-ipu-channel/m-p/689750#M106829</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-18T23:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: linux kernel is halt when open the ipu_channel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-kernel-is-halt-when-open-the-ipu-channel/m-p/689751#M106830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;BR /&gt; Thank you very much for your reply.Later I test and add some log message into kernel source code by myself, print the message, I forget to say I connect the IPU-CSI interface to FPGA,and FPGA send a lot of generic data to the IPU and running on the GATED_CLK mode,run the driver and later the kernel is stop.It seems that really stop because i remove and reinstall the sdcard but the kernel was not active at all, it is the last runtime log message of the kernel below:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;enter ipu_err_irq_handler().IRQ:37&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;end ipu_err_irq_handler(),IRQ&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;enter ipu_err_irq_handler.IRQ:37&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;end ipu_err_irq_handler(),IRQ()&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;call ipu_dump_registers&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;imx-ipuv3 2400000.ipu: IPU_CONF = 0x00000101&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I think it is not a hardware problem, according to the log message, we can see that the registers value,&lt;STRONG&gt;IPU_INT_STAT_10 is 0x1,&amp;nbsp;&lt;/STRONG&gt;refer to the manual, &lt;STRONG&gt;&lt;SPAN class=""&gt;This bit indicates on an interrupt that is a result of a result of a Frame Lost of SMFC channel 0,&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN class=""&gt; and the&amp;nbsp;&lt;STRONG&gt;IPU_INT_STAT_5 is 0x1, &lt;SPAN class=""&gt;New Frame before end-of-frame error indication of Channel interrupt. This bit is the status bit of New&amp;nbsp;Frame before end-of-frame error interrupt of Channel #n.&lt;/SPAN&gt; &lt;BR style="font-weight: normal;" /&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;and I dump the ipu registers but no fully because the kernal is stop, I think the problem is my configuration &amp;nbsp;error or mistake some config on ipu,but I think the kernel should not be stop.&amp;nbsp;but i don't know how to fixed it, I search a lot of document but no found on google and baidu research, please help me, thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jun 2017 03:05:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-kernel-is-halt-when-open-the-ipu-channel/m-p/689751#M106830</guid>
      <dc:creator>wwfdzh2012</dc:creator>
      <dc:date>2017-06-19T03:05:24Z</dc:date>
    </item>
  </channel>
</rss>