<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can imx6dual encode continuous RGB bitmaps to H264 video stream? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6dual-encode-continuous-RGB-bitmaps-to-H264-video-stream/m-p/687370#M106395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can imx6dual encode continuous RGB bitmaps to H264 video stream? The RGB bitmaps is received from eithernet ,15 frames per second,320*256 pixels,and the H264 video stream is send out through wifi.This is to say,the imx6dual is used to encode BMPs to H264 video.Can imx6dual do this? If can,how to realize?Please give me some adivce.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 21 May 2017 01:48:51 GMT</pubDate>
    <dc:creator>zoushx</dc:creator>
    <dc:date>2017-05-21T01:48:51Z</dc:date>
    <item>
      <title>Can imx6dual encode continuous RGB bitmaps to H264 video stream?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6dual-encode-continuous-RGB-bitmaps-to-H264-video-stream/m-p/687370#M106395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can imx6dual encode continuous RGB bitmaps to H264 video stream? The RGB bitmaps is received from eithernet ,15 frames per second,320*256 pixels,and the H264 video stream is send out through wifi.This is to say,the imx6dual is used to encode BMPs to H264 video.Can imx6dual do this? If can,how to realize?Please give me some adivce.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 May 2017 01:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6dual-encode-continuous-RGB-bitmaps-to-H264-video-stream/m-p/687370#M106395</guid>
      <dc:creator>zoushx</dc:creator>
      <dc:date>2017-05-21T01:48:51Z</dc:date>
    </item>
    <item>
      <title>Re: Can imx6dual encode continuous RGB bitmaps to H264 video stream?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6dual-encode-continuous-RGB-bitmaps-to-H264-video-stream/m-p/687371#M106396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zou&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for supported formats please refer to sect.3.2.2 Data and Structure Definitions&lt;/P&gt;&lt;P&gt;attached VPU Linux Guide. In general one can try to use CSC with examples described on&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fdocs%2FDOC-94961" rel="nofollow" target="_blank"&gt;https://community.freescale.com/docs/DOC-94961&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 May 2017 23:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6dual-encode-continuous-RGB-bitmaps-to-H264-video-stream/m-p/687371#M106396</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-21T23:51:03Z</dc:date>
    </item>
  </channel>
</rss>