<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SabreSD boot from eMMC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687325#M106393</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;thanks for the reply. As mentioned above, I actually did use the mfgtool2 to download the demo image, and it seems to work also as I can see the eMMC contains the image files and rootfs.&lt;/P&gt;&lt;P&gt;Is there anything I can debug further to know whether it is a hardware fault or not?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Jul 2017 13:34:02 GMT</pubDate>
    <dc:creator>lhwr</dc:creator>
    <dc:date>2017-07-10T13:34:02Z</dc:date>
    <item>
      <title>SabreSD boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687323#M106391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am having issue on booting my MCIMX6Q-SDB/SabreSD board from the on-board eMMC (uSDHC4). I have used the MfgTool to flash u-boot, linux kernel, dtb, and rootfs into the eMMC, and it seems to work without error. However setting the SW6 to 010xxx11 (msb-&amp;gt;lsb), I can't see the board booting at all. I can see u-boot working when using SD Card attached to SD3(J507)/SD2(J500) on the board by setting SW6 to 010xxx01/010xxx10 and even boot the linux kernel from SD card attached SD2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the system boots from SD2, I tried to examine the attached devices, I can see that the eMMC is listed under /dev and event mounted by the system:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# ls -l /dev/mmcblk*&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp;&amp;nbsp; 0 Apr&amp;nbsp; 5 00:15 /dev/mmcblk0&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp;&amp;nbsp; 1 Apr&amp;nbsp; 5 00:15 /dev/mmcblk0p1&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp;&amp;nbsp; 2 Apr&amp;nbsp; 5 00:15 /dev/mmcblk0p2&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp;&amp;nbsp; 8 Apr&amp;nbsp; 5 00:15 /dev/mmcblk1&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp; 16 Apr&amp;nbsp; 5 00:15 /dev/mmcblk1boot0&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp; 24 Apr&amp;nbsp; 5 00:15 /dev/mmcblk1boot1&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp;&amp;nbsp; 9 Apr&amp;nbsp; 5 00:15 /dev/mmcblk1p1&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp; 10 Apr&amp;nbsp; 5 00:15 /dev/mmcblk1p2&lt;BR /&gt;brw-rw----&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 179,&amp;nbsp; 32 Apr&amp;nbsp; 5 00:15 /dev/mmcblk1rpmb&lt;BR /&gt;root@imx6qdlsolo:~# mount&lt;BR /&gt;rootfs on / type rootfs (rw)&lt;BR /&gt;/dev/root on / type ext3 (rw,relatime,errors=continue,user_xattr,acl,barrier=1,data=ordered)&lt;BR /&gt;devtmpfs on /dev type devtmpfs (rw,relatime,size=348840k,nr_inodes=87210,mode=755)&lt;BR /&gt;proc on /proc type proc (rw,relatime)&lt;BR /&gt;tmpfs on /mnt/.psplash type tmpfs (rw,relatime,size=40k)&lt;BR /&gt;sysfs on /sys type sysfs (rw,relatime)&lt;BR /&gt;debugfs on /sys/kernel/debug type debugfs (rw,relatime)&lt;BR /&gt;tmpfs on /run type tmpfs (rw,nosuid,nodev,mode=755)&lt;BR /&gt;tmpfs on /var/volatile type tmpfs (rw,relatime)&lt;BR /&gt;devpts on /dev/pts type devpts (rw,relatime,gid=5,mode=620)&lt;BR /&gt;/dev/mmcblk1p2 on /media/mmcblk1p2 type ext4 (rw,relatime,data=ordered)&lt;BR /&gt;/dev/mmcblk1p1 on /media/mmcblk1p1 type vfat (rw,relatime,gid=6,fmask=0007,dmask=0007,allow_utime=0020,codepage=437,iocharset=iso8859-1,shortname=mixed,errors=remount-ro)&lt;BR /&gt;/dev/mmcblk0p1 on /media/mmcblk0p1 type vfat (rw,relatime,gid=6,fmask=0007,dmask=0007,allow_utime=0020,codepage=437,iocharset=iso8859-1,shortname=mixed,errors=remount-ro)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;its partitions even seems to contain correct files (FAT first partition containing kernel image and DTB, ext4 second partition containing rootfs):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# ls -l /media/mmcblk1p1&lt;BR /&gt;-rwxrwx---&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 47179 Jan&amp;nbsp; 1&amp;nbsp; 1980 imx6dl-sabresd.dtb&lt;BR /&gt;-rwxrwx---&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 47179 Jan&amp;nbsp; 1&amp;nbsp; 1980 imx6q-sabresd.dtb&lt;BR /&gt;-rwxrwx---&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; disk&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5260936 Jan&amp;nbsp; 1&amp;nbsp; 1980 uImage&lt;BR /&gt;root@imx6qdlsolo:~# ls -l /media/mmcblk1p2&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 bin&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 boot&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 dev&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp; 44 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 etc&lt;BR /&gt;drwxr-sr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 4 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 home&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 7 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 lib&lt;BR /&gt;drwx------&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16384 Jan&amp;nbsp; 1&amp;nbsp; 1970 lost+found&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Apr&amp;nbsp; 4 22:42 media&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 3 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 mnt&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 6 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 opt&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Apr&amp;nbsp; 4 22:42 proc&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Apr&amp;nbsp; 4 22:42 run&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 sbin&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Apr&amp;nbsp; 4 22:42 sys&lt;BR /&gt;drwxrwxrwt&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Apr&amp;nbsp; 4 22:42 tmp&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 2 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 unit_tests&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp; 11 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 usr&lt;BR /&gt;drwxr-xr-x&amp;nbsp;&amp;nbsp;&amp;nbsp; 8 root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4096 Jan&amp;nbsp; 1&amp;nbsp; 1970 var&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I event checked whether the IVT is correctly installed:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# hexdump -C -n 32 -s 1024 /dev/mmcblk1&lt;BR /&gt;00000400&amp;nbsp; d1 00 20 40 00 00 80 17&amp;nbsp; 00 00 00 00 2c b0 7f 17&amp;nbsp; |.. @........,...|&lt;BR /&gt;00000410&amp;nbsp; 20 b0 7f 17 00 b0 7f 17&amp;nbsp; 00 00 00 00 00 00 00 00&amp;nbsp; | ...............|&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Everything seems to look fine. So the question is what can I do to debug why booting from the eMMC is not working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 09:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687323#M106391</guid>
      <dc:creator>lhwr</dc:creator>
      <dc:date>2017-07-07T09:04:35Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687324#M106392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try with Demo Images&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=13376994…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and MFG Tools&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=13376…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;use mfgtool2-yocto-mx-sabresd-emmc.vbs script&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 23:29:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687324#M106392</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-07T23:29:27Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687325#M106393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;thanks for the reply. As mentioned above, I actually did use the mfgtool2 to download the demo image, and it seems to work also as I can see the eMMC contains the image files and rootfs.&lt;/P&gt;&lt;P&gt;Is there anything I can debug further to know whether it is a hardware fault or not?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jul 2017 13:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687325#M106393</guid>
      <dc:creator>lhwr</dc:creator>
      <dc:date>2017-07-10T13:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: SabreSD boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687326#M106394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can attach jtag debugger and dump 0x907400 (ROM uses 0x907000 as starting address),&lt;BR /&gt;one should see IVT header here if the emmc access is ok. Similar procedure is described on&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fthread%2F307723" rel="nofollow" target="_blank"&gt;https://community.freescale.com/thread/307723&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jul 2017 23:25:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-boot-from-eMMC/m-p/687326#M106394</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-10T23:25:00Z</dc:date>
    </item>
  </channel>
</rss>