<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The kernel 3.14.52  hang-up in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-kernel-3-14-52-hang-up/m-p/687141#M106356</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this may be due to ddr errors, please try ddr test on&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-105652"&gt;https://community.nxp.com/docs/DOC-105652 &lt;/A&gt;&lt;/P&gt;&lt;P&gt;and update image with new calibration coefficients found from that test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Aug 2017 23:18:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-08-02T23:18:55Z</dc:date>
    <item>
      <title>The kernel 3.14.52  hang-up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-kernel-3-14-52-hang-up/m-p/687140#M106355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use i.MX6q,and the kernel 3.14.52,sometimes kernel will print some warning information is below, and sometimes this warning will &amp;nbsp;cause the system hang-up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# [ 1420.451781] BUG: scheduling while atomic: swapper/1/0/0x00000002&lt;BR /&gt;[ 1420.451855] Modules linked in: ipt_MASQUERADE xt_tcpudp xt_limit xt_conntrack iptable_nat nf_conntrack_ipv4 nf_defrag_ipv4 nf_nat_ipv4 nf_nat nf_conntrack iptable_filter ip_tables x_tables lsm9ds1_acc_gyr ds90ub925q ds90ub926q mxc_dcic&lt;BR /&gt;[ 1420.451872] CPU: 1 PID: 0 Comm: swapper/1 Tainted: G W 3.14.52-rt52 #4&lt;BR /&gt;[ 1420.451929] [&amp;lt;800149b8&amp;gt;] (unwind_backtrace) from [&amp;lt;80011740&amp;gt;] (show_stack+0x10/0x14)&lt;BR /&gt;[ 1420.451966] [&amp;lt;80011740&amp;gt;] (show_stack) from [&amp;lt;8068a064&amp;gt;] (dump_stack+0x98/0xdc)&lt;BR /&gt;[ 1420.451993] [&amp;lt;8068a064&amp;gt;] (dump_stack) from [&amp;lt;80687b0c&amp;gt;] (__schedule_bug+0x50/0x64)&lt;BR /&gt;[ 1420.452016] [&amp;lt;80687b0c&amp;gt;] (__schedule_bug) from [&amp;lt;8068c888&amp;gt;] (__schedule+0x45c/0x480)&lt;BR /&gt;[ 1420.452037] [&amp;lt;8068c888&amp;gt;] (__schedule) from [&amp;lt;8068c8ec&amp;gt;] (schedule+0x40/0xbc)&lt;BR /&gt;[ 1420.452058] [&amp;lt;8068c8ec&amp;gt;] (schedule) from [&amp;lt;8068e030&amp;gt;] (rt_spin_lock_slowlock+0x12c/0x254)&lt;BR /&gt;[ 1420.452096] [&amp;lt;8068e030&amp;gt;] (rt_spin_lock_slowlock) from [&amp;lt;804997ec&amp;gt;] (choose_freq.isra.19+0x40/0x1b8)&lt;BR /&gt;[ 1420.452118] [&amp;lt;804997ec&amp;gt;] (choose_freq.isra.19) from [&amp;lt;80499a74&amp;gt;] (cpufreq_interactive_timer+0x110/0x358)&lt;BR /&gt;[ 1420.452135] [&amp;lt;80499a74&amp;gt;] (cpufreq_interactive_timer) from [&amp;lt;80499d58&amp;gt;] (cpufreq_interactive_idle_notifier+0x9c/0x120)&lt;BR /&gt;[ 1420.452166] [&amp;lt;80499d58&amp;gt;] (cpufreq_interactive_idle_notifier) from [&amp;lt;8004a824&amp;gt;] (notifier_call_chain+0x44/0x84)&lt;BR /&gt;[ 1420.452191] [&amp;lt;8004a824&amp;gt;] (notifier_call_chain) from [&amp;lt;8004aab8&amp;gt;] (atomic_notifier_call_chain+0x34/0x48)&lt;BR /&gt;[ 1420.452219] [&amp;lt;8004aab8&amp;gt;] (atomic_notifier_call_chain) from [&amp;lt;80069b6c&amp;gt;] (cpu_startup_entry+0xdc/0x180)&lt;BR /&gt;[ 1420.452242] [&amp;lt;80069b6c&amp;gt;] (cpu_startup_entry) from [&amp;lt;100085c4&amp;gt;] (0x100085c4)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you give me some advice? or&amp;nbsp;Someone else &amp;nbsp;meet &amp;nbsp;the same problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 11:01:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-kernel-3-14-52-hang-up/m-p/687140#M106355</guid>
      <dc:creator>janyonggang</dc:creator>
      <dc:date>2017-07-28T11:01:21Z</dc:date>
    </item>
    <item>
      <title>Re: The kernel 3.14.52  hang-up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-kernel-3-14-52-hang-up/m-p/687141#M106356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this may be due to ddr errors, please try ddr test on&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-105652"&gt;https://community.nxp.com/docs/DOC-105652 &lt;/A&gt;&lt;/P&gt;&lt;P&gt;and update image with new calibration coefficients found from that test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 23:18:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-kernel-3-14-52-hang-up/m-p/687141#M106356</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-02T23:18:55Z</dc:date>
    </item>
  </channel>
</rss>