<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Queries on IMX6ULL processor GPIO pin. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685962#M106134</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am just using Ohms law to determine the current for the GPIO when its 3.3V IO logic, Drive current form 20mA to 140mA as per "4.8.1 Single Voltage GPIO Output Buffer Impedance" in the datasheet. Am i right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And we are going to use GPIO in sourcing power to the LED for Indication use case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,RK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 May 2017 06:37:21 GMT</pubDate>
    <dc:creator>ramesh6663</dc:creator>
    <dc:date>2017-05-19T06:37:21Z</dc:date>
    <item>
      <title>Queries on IMX6ULL processor GPIO pin.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685960#M106132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Could you please let me know the Maximum drive current of IMX6ULL GPIO pin from Processor? &amp;nbsp;I believe its &amp;gt;10mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;So please confirm&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 May 2017 05:13:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685960#M106132</guid>
      <dc:creator>ramesh6663</dc:creator>
      <dc:date>2017-05-19T05:13:07Z</dc:date>
    </item>
    <item>
      <title>Re: Queries on IMX6ULL processor GPIO pin.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685961#M106133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; The GPIO buffer load capacity is not specified in units of current. It is specified in terms of buffer drive strength or output impedance. For example, refer to the Section "GPIO Output Buffer Impedance" of the i.MX 6ULL Data Sheet(s).&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;IBIS models may be used to estimate current.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/395489"&gt;https://community.nxp.com/message/395489&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Also, the total load current and power dissipation should be taken into account when calculating the GPIO power budget.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 May 2017 05:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685961#M106133</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-05-19T05:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: Queries on IMX6ULL processor GPIO pin.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685962#M106134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am just using Ohms law to determine the current for the GPIO when its 3.3V IO logic, Drive current form 20mA to 140mA as per "4.8.1 Single Voltage GPIO Output Buffer Impedance" in the datasheet. Am i right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And we are going to use GPIO in sourcing power to the LED for Indication use case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,RK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 May 2017 06:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685962#M106134</guid>
      <dc:creator>ramesh6663</dc:creator>
      <dc:date>2017-05-19T06:37:21Z</dc:date>
    </item>
    <item>
      <title>Re: Queries on IMX6ULL processor GPIO pin.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685963#M106135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You should take into account LED volt ampere characteristic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/381665"&gt;https://community.nxp.com/message/381665&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 May 2017 07:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Queries-on-IMX6ULL-processor-GPIO-pin/m-p/685963#M106135</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-05-19T07:08:07Z</dc:date>
    </item>
  </channel>
</rss>