<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: QtCreator SFTP initialization failed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QtCreator-SFTP-initialization-failed/m-p/685377#M106021</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Sahin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can follow the bellow steps may be helpful to you.&lt;/P&gt;&lt;P&gt;1. switch to Projects mode (Ctrl-4)&lt;BR /&gt; 2. for board kit choose Run tab&lt;BR /&gt; 3. in Deployment settings disable step "Upload files via SFTP"&lt;BR /&gt; 4. push the button "Add Deploy Step"&lt;BR /&gt; 5. choose "Custom Process Step"&lt;BR /&gt; 6. write in Command: scp&lt;BR /&gt; 7. write in Arguments: local_file_path &lt;A href="mailto:root@your"&gt;root@ you&lt;/A&gt; _board_ip:board_remote_directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you find any other answer please share it here.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Nandish sg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jul 2017 05:26:08 GMT</pubDate>
    <dc:creator>nandishguruling</dc:creator>
    <dc:date>2017-07-28T05:26:08Z</dc:date>
    <item>
      <title>QtCreator SFTP initialization failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QtCreator-SFTP-initialization-failed/m-p/685376#M106020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I have tried to upload a new program so click the run button through QtCreator to imx6SoloX Sabre Board but get an error that is "SFTP initialization failed". I can connect the device successfully. How can I solve this problem?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6Solox Linux Kernel :&amp;nbsp;3.10.53-1.1.0_ga+g496fbe0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Compile Output:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;13:33:04: Running steps for project deneme...&lt;BR /&gt;13:33:04: Configuration unchanged, skipping qmake step.&lt;BR /&gt;13:33:04: Starting: "/usr/bin/make" &lt;BR /&gt;make: Nothing to be done for `first'.&lt;BR /&gt;13:33:04: The process "/usr/bin/make" exited normally.&lt;BR /&gt;13:33:04: Connecting to device...&lt;BR /&gt;13:33:05: The remote file system has 148 megabytes of free space, going ahead.&lt;BR /&gt;13:33:05: Deploy step finished.&lt;BR /&gt;13:33:05: SFTP initialization failed: The SFTP server finished unexpectedly with exit code 127.&lt;BR /&gt;13:33:05: Deploy step failed.&lt;BR /&gt;Error while building/deploying project deneme (kit: imx SoloX)&lt;BR /&gt;When executing step "Upload files via SFTP"&lt;BR /&gt;13:33:05: Elapsed time: 00:00.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Device Test:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Connecting to host...&lt;BR /&gt;Checking kernel version...&lt;BR /&gt;Linux 3.10.53-1.1.0_ga+g496fbe0 armv7l&lt;/P&gt;&lt;P&gt;Checking if specified ports are available...&lt;BR /&gt;All specified ports are available.&lt;/P&gt;&lt;P&gt;Device test finished successfully.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 10:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QtCreator-SFTP-initialization-failed/m-p/685376#M106020</guid>
      <dc:creator>gokhansahin</dc:creator>
      <dc:date>2017-07-06T10:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: QtCreator SFTP initialization failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QtCreator-SFTP-initialization-failed/m-p/685377#M106021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Sahin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can follow the bellow steps may be helpful to you.&lt;/P&gt;&lt;P&gt;1. switch to Projects mode (Ctrl-4)&lt;BR /&gt; 2. for board kit choose Run tab&lt;BR /&gt; 3. in Deployment settings disable step "Upload files via SFTP"&lt;BR /&gt; 4. push the button "Add Deploy Step"&lt;BR /&gt; 5. choose "Custom Process Step"&lt;BR /&gt; 6. write in Command: scp&lt;BR /&gt; 7. write in Arguments: local_file_path &lt;A href="mailto:root@your"&gt;root@ you&lt;/A&gt; _board_ip:board_remote_directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you find any other answer please share it here.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Nandish sg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 05:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QtCreator-SFTP-initialization-failed/m-p/685377#M106021</guid>
      <dc:creator>nandishguruling</dc:creator>
      <dc:date>2017-07-28T05:26:08Z</dc:date>
    </item>
  </channel>
</rss>