<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MX7D QSPI Configuration for MX66L1G45G in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX7D-QSPI-Configuration-for-MX66L1G45G/m-p/685256#M105988</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MX66 flash works with MX25 config file. We had a reset problem, flash was held in reset after power up. Now booting from qpi works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Jun 2017 19:02:14 GMT</pubDate>
    <dc:creator>dietersteininge</dc:creator>
    <dc:date>2017-06-21T19:02:14Z</dc:date>
    <item>
      <title>MX7D QSPI Configuration for MX66L1G45G</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7D-QSPI-Configuration-for-MX66L1G45G/m-p/685254#M105986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Programming QSPI flash is possible on our customer board with mfg tool an i think, the fuses are set correct (HW_OCOTP_BOOT_CFG0 = 0x10004000, Boot_mode is 00). The QSPI flash was accessed after reboot, but nothing more happens (no console output).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe there´s a problem with the qspi config file (i still use the original qspi-nor-macronix-mx25l51245g-config file). Is a modified config file for the MX66L1G45G available/necessary?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 15:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7D-QSPI-Configuration-for-MX66L1G45G/m-p/685254#M105986</guid>
      <dc:creator>dietersteininge</dc:creator>
      <dc:date>2017-06-13T15:00:25Z</dc:date>
    </item>
    <item>
      <title>Re: MX7D QSPI Configuration for MX66L1G45G</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7D-QSPI-Configuration-for-MX66L1G45G/m-p/685255#M105987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dieter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately I am not aware of config file for the MX66L1G45G, just for test one can try to&lt;/P&gt;&lt;P&gt;boot for example in single mode of operation, also check if uboot has support for that flash&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.mail-archive.com/u-boot@lists.denx.de/msg229045.html" title="https://www.mail-archive.com/u-boot@lists.denx.de/msg229045.html"&gt;Re: [U-Boot] [PATCH] spi: Add support for MX66U51235F, MX66L1G45G and MT25QU02G&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;attach jtag debugger and dump 0x910400 (ROM uses 0x910000 as starting address),&lt;BR /&gt;you should see ivt header here if the qspi access is ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 00:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7D-QSPI-Configuration-for-MX66L1G45G/m-p/685255#M105987</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-14T00:46:20Z</dc:date>
    </item>
    <item>
      <title>Re: MX7D QSPI Configuration for MX66L1G45G</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7D-QSPI-Configuration-for-MX66L1G45G/m-p/685256#M105988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MX66 flash works with MX25 config file. We had a reset problem, flash was held in reset after power up. Now booting from qpi works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 19:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7D-QSPI-Configuration-for-MX66L1G45G/m-p/685256#M105988</guid>
      <dc:creator>dietersteininge</dc:creator>
      <dc:date>2017-06-21T19:02:14Z</dc:date>
    </item>
  </channel>
</rss>