<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How much is the power consumption for RTC?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-much-is-the-power-consumption-for-RTC/m-p/685212#M105980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jacopo Agostini,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RTC power consumption on the datasheet is correct and furthermore is a typical value, not the maximum possible RTC power consumption, which means it may be higher than that.&lt;/P&gt;&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Jun 2017 21:10:02 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-06-14T21:10:02Z</dc:date>
    <item>
      <title>How much is the power consumption for RTC?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-much-is-the-power-consumption-for-RTC/m-p/685211#M105979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I wanted to know how the i.MX6UL handles the RTC. From the datasheet I seem to have understood&amp;nbsp;that the RTC power consumption to be on is in the order of hundred of uA. In my PCB there is no space for a coin cell so I want to use a supercap to supply the RTC even when all system is off. The problem is that in this case the duration of the supercap is much lower than a coin cell because of the elevated RTC power consumption; so I want to ask if the RTC power consumption is really so excessive that I'm not allowed to use a Supercap.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 14:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-much-is-the-power-consumption-for-RTC/m-p/685211#M105979</guid>
      <dc:creator>jacopoagostini</dc:creator>
      <dc:date>2017-06-13T14:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: How much is the power consumption for RTC?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-much-is-the-power-consumption-for-RTC/m-p/685212#M105980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jacopo Agostini,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RTC power consumption on the datasheet is correct and furthermore is a typical value, not the maximum possible RTC power consumption, which means it may be higher than that.&lt;/P&gt;&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 21:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-much-is-the-power-consumption-for-RTC/m-p/685212#M105980</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-06-14T21:10:02Z</dc:date>
    </item>
  </channel>
</rss>