<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RGB display, screen flipped vertically. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685025#M105936</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuva&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes it uses PxP, could you try with lcd provided with i.MX7D Sabre SD - LCD8000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Jul 2017 06:44:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-07-06T06:44:55Z</dc:date>
    <item>
      <title>RGB display, screen flipped vertically.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685021#M105932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a RGB interface display of 45 pins which we have connected to the iMX7 sabre board with a adapter since the RGB interface on the sabre is 50 pins. I have set the &amp;nbsp;lcdif device tree to configure the display as below based on the display data sheet. but the display seems to be flipped vertically (mirrored vertically, picture attached). Has anyone faced similar issue? is there any setting in the driver that I am missing that needs to be set for the RGB interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;lcdif {&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_lcdif_dat&lt;BR /&gt; &amp;amp;pinctrl_lcdif_ctrl&amp;gt;;&lt;BR /&gt; enable-gpio = &amp;lt;&amp;amp;gpio_spi 7 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt; display = &amp;lt;&amp;amp;display0&amp;gt;;&lt;BR /&gt; status = "okay";&lt;/P&gt;&lt;P&gt;display0: display {&lt;BR /&gt; bits-per-pixel = &amp;lt;24&amp;gt;;&lt;BR /&gt; bus-width = &amp;lt;24&amp;gt;;&lt;/P&gt;&lt;P&gt;display-timings {&lt;BR /&gt; native-mode = &amp;lt;&amp;amp;timing_wvga&amp;gt;;&lt;BR /&gt; /* WVGA Timing*/&lt;BR /&gt; timing_wvga: 800x480 {&lt;BR /&gt; clock-frequency = &amp;lt;33300000&amp;gt;;&lt;BR /&gt; hactive = &amp;lt;800&amp;gt;;&lt;BR /&gt; vactive = &amp;lt;480&amp;gt;;&lt;BR /&gt; hback-porch = &amp;lt;46&amp;gt;;&lt;BR /&gt; hfront-porch = &amp;lt;210&amp;gt;;&lt;BR /&gt; vback-porch = &amp;lt;23&amp;gt;;&lt;BR /&gt; vfront-porch = &amp;lt;22&amp;gt;;&lt;BR /&gt; hsync-len = &amp;lt;20&amp;gt;;&lt;BR /&gt; vsync-len = &amp;lt;10&amp;gt;;&lt;/P&gt;&lt;P&gt;de-active = &amp;lt;1&amp;gt;;&lt;BR /&gt; hsync-active = &amp;lt;0&amp;gt;;&lt;BR /&gt; vsync-active = &amp;lt;0&amp;gt;;&lt;BR /&gt; pixelclk-active = &amp;lt;1&amp;gt;;&lt;BR /&gt; };&lt;BR /&gt; };&lt;BR /&gt; };&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/imx7s lcd/tg-p"&gt;#imx7s lcd&lt;/A&gt;‌ &lt;A href="https://community.nxp.com/t5/tag/imx7s display/tg-p"&gt;#imx7s display&lt;/A&gt;‌ &lt;A href="https://community.nxp.com/t5/tag/RGB/tg-p"&gt;#RGB&lt;/A&gt;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/tag/RGBinterface/tg-p"&gt;#RGBinterface&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2017 23:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685021#M105932</guid>
      <dc:creator>czur</dc:creator>
      <dc:date>2017-07-05T23:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: RGB display, screen flipped vertically.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685022#M105933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to flip image using example in unit tests (imx-test):&lt;/P&gt;&lt;P&gt;..test/pxp_lib_test/pxp_test.c&lt;BR /&gt;&lt;A href="https://community.nxp.com/www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz" target="test_blank"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 05:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685022#M105933</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-06T05:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: RGB display, screen flipped vertically.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685023#M105934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By Default if we have the IMX7 connected to 45 Pin RGB Display, why it should show the image as flipped in attached image.&amp;nbsp; Isn't it a issue with IMX7 RGB Driver or Framebuffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per the question it says the configuration isn't changed other than Device Tree.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By Default, does the RGB Display Driver uses PXP? How can we use the test to fix this concern.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Yuva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 05:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685023#M105934</guid>
      <dc:creator>yuvakrishna</dc:creator>
      <dc:date>2017-07-06T05:59:46Z</dc:date>
    </item>
    <item>
      <title>Re: RGB display, screen flipped vertically.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685024#M105935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can check with the u-boot parameters, while booting time press any key, and type print now see the displayinfo arguments,Like&amp;nbsp; (example"displayinfo Video=mxcfbo ,dev=lcd ,800x480@70,if=RGB565"), set these arguments according to your display,&lt;/P&gt;&lt;P&gt;i hope your display x=800 and y=480 (i.e 800x480 ) then according to this what you got that is correct format only,&lt;/P&gt;&lt;P&gt;if you get any other answer please share it here,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;SGN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 06:07:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685024#M105935</guid>
      <dc:creator>nandishguruling</dc:creator>
      <dc:date>2017-07-06T06:07:38Z</dc:date>
    </item>
    <item>
      <title>Re: RGB display, screen flipped vertically.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685025#M105936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuva&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes it uses PxP, could you try with lcd provided with i.MX7D Sabre SD - LCD8000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 06:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685025#M105936</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-06T06:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: RGB display, screen flipped vertically.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685026#M105937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;By Default, does the RGB Display Driver uses PXP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you try with lcd provided with i.MX7D Sabre SD - LCD8000 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 11:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685026#M105937</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-06T11:23:55Z</dc:date>
    </item>
    <item>
      <title>Re: RGB display, screen flipped vertically.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685027#M105938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seems like the issue was with the Display controller jumper setting's. The scan direction was set wrong.&lt;/P&gt;&lt;P&gt;but the PXP example is useful in understanding the usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Igor!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2017 21:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGB-display-screen-flipped-vertically/m-p/685027#M105938</guid>
      <dc:creator>czur</dc:creator>
      <dc:date>2017-07-14T21:23:55Z</dc:date>
    </item>
  </channel>
</rss>