<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6Q reboot hangs issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-reboot-hangs-issue/m-p/684972#M105917</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use "fsl-yocto-L4.1.15_2.0.0-ga" BSP of imx6q. However, when I enter reboot command, the debug port shows as the following:&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# reboot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The system is going down for reboot NOW! (ttymxc0) (Mon Jun 12 08:15:47 2017)&lt;BR /&gt;INIT: Switching to runlevel: 6&lt;BR /&gt;INIT: Sending processes the TERM signal&lt;BR /&gt;root@imx6qsabresd:~# Stopping XServer&lt;BR /&gt;Stopping Dropbear SSH server: stopped /usr/sbin/dropbear (pid 599)&lt;BR /&gt;dropbear.&lt;BR /&gt;&amp;nbsp;* Stopping Avahi mDNS/DNS-SD Daemon: avahi-daemon&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ ok ]&lt;BR /&gt;Stopping advanced power management daemon: no /usr/sbin/apmd found; none killed&lt;BR /&gt;apmd.&lt;BR /&gt;Stopping atd: OK&lt;BR /&gt;Stopping bluetooth&lt;BR /&gt;/usr/libexec/bluetooth/bluetoothd&lt;BR /&gt;Stopping system message bus: dbus.&lt;BR /&gt;stopping mountd: done&lt;BR /&gt;stopping nfsd: done&lt;BR /&gt;Stopping ntpd: done&lt;BR /&gt;Stopping system log daemon...0&lt;BR /&gt;Stopping kernel log daemon...0&lt;BR /&gt;stopping statd: done&lt;BR /&gt;Stopping Connection Manager&lt;BR /&gt;Stopping Telephony daemon&lt;BR /&gt;ALSA: Storing mixer settings...&lt;BR /&gt;/usr/sbin/alsactl: save_state:1595: No soundcards found...&lt;BR /&gt;Stopping crond: OK&lt;BR /&gt;Stopping rpcbind daemon...&lt;BR /&gt;done.&lt;BR /&gt;Stopping Linux NFC daemon&lt;BR /&gt;Deconfiguring network interfaces... done.&lt;BR /&gt;Sending all processes the TERM signal...&lt;BR /&gt;logout&lt;BR /&gt;Sending all processes the KILL signal...&lt;BR /&gt;Unmounting remote filesystems...&lt;BR /&gt;Deactivating swap...&lt;BR /&gt;Unmounting local filesystems...&lt;BR /&gt;EXT4-fs (mmcblk3p2): re-mounted. Opts: (null)&lt;BR /&gt;Rebooting... reboot: Restarting system&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then the system hangs and will not reboot at all. Our board is designed based on imx6q sabresd, but without WDOG_B signal connecting to external PMIC. I want to confirm whether it is necessary for the system. BTW we use ldo_enable in our board design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you everybody!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2017 05:59:45 GMT</pubDate>
    <dc:creator>caritzhu</dc:creator>
    <dc:date>2017-06-13T05:59:45Z</dc:date>
    <item>
      <title>iMX6Q reboot hangs issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-reboot-hangs-issue/m-p/684972#M105917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use "fsl-yocto-L4.1.15_2.0.0-ga" BSP of imx6q. However, when I enter reboot command, the debug port shows as the following:&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# reboot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The system is going down for reboot NOW! (ttymxc0) (Mon Jun 12 08:15:47 2017)&lt;BR /&gt;INIT: Switching to runlevel: 6&lt;BR /&gt;INIT: Sending processes the TERM signal&lt;BR /&gt;root@imx6qsabresd:~# Stopping XServer&lt;BR /&gt;Stopping Dropbear SSH server: stopped /usr/sbin/dropbear (pid 599)&lt;BR /&gt;dropbear.&lt;BR /&gt;&amp;nbsp;* Stopping Avahi mDNS/DNS-SD Daemon: avahi-daemon&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [ ok ]&lt;BR /&gt;Stopping advanced power management daemon: no /usr/sbin/apmd found; none killed&lt;BR /&gt;apmd.&lt;BR /&gt;Stopping atd: OK&lt;BR /&gt;Stopping bluetooth&lt;BR /&gt;/usr/libexec/bluetooth/bluetoothd&lt;BR /&gt;Stopping system message bus: dbus.&lt;BR /&gt;stopping mountd: done&lt;BR /&gt;stopping nfsd: done&lt;BR /&gt;Stopping ntpd: done&lt;BR /&gt;Stopping system log daemon...0&lt;BR /&gt;Stopping kernel log daemon...0&lt;BR /&gt;stopping statd: done&lt;BR /&gt;Stopping Connection Manager&lt;BR /&gt;Stopping Telephony daemon&lt;BR /&gt;ALSA: Storing mixer settings...&lt;BR /&gt;/usr/sbin/alsactl: save_state:1595: No soundcards found...&lt;BR /&gt;Stopping crond: OK&lt;BR /&gt;Stopping rpcbind daemon...&lt;BR /&gt;done.&lt;BR /&gt;Stopping Linux NFC daemon&lt;BR /&gt;Deconfiguring network interfaces... done.&lt;BR /&gt;Sending all processes the TERM signal...&lt;BR /&gt;logout&lt;BR /&gt;Sending all processes the KILL signal...&lt;BR /&gt;Unmounting remote filesystems...&lt;BR /&gt;Deactivating swap...&lt;BR /&gt;Unmounting local filesystems...&lt;BR /&gt;EXT4-fs (mmcblk3p2): re-mounted. Opts: (null)&lt;BR /&gt;Rebooting... reboot: Restarting system&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then the system hangs and will not reboot at all. Our board is designed based on imx6q sabresd, but without WDOG_B signal connecting to external PMIC. I want to confirm whether it is necessary for the system. BTW we use ldo_enable in our board design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you everybody!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 05:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-reboot-hangs-issue/m-p/684972#M105917</guid>
      <dc:creator>caritzhu</dc:creator>
      <dc:date>2017-06-13T05:59:45Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q reboot hangs issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-reboot-hangs-issue/m-p/684973#M105918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi carit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is expected behaviour as without without WDOG_B resetting&lt;/P&gt;&lt;P&gt;whole board power, processor may start to boot with lower VDD_ARM_IN&lt;/P&gt;&lt;P&gt;voltages, as cpu freq driver may set it to low values. One can try&lt;/P&gt;&lt;P&gt;to disable cpu freq driver or guarantee valid VDD_ARM_IN value&lt;/P&gt;&lt;P&gt;at reboot by any other ways.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 10:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-reboot-hangs-issue/m-p/684973#M105918</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-13T10:28:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q reboot hangs issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-reboot-hangs-issue/m-p/684974#M105919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply!&lt;/P&gt;&lt;P&gt;I think you are right, the CPU may occur issue when restart with 400M low freq. And if I set cpu freq to be 996MHz by using the command of "echo 996000 &amp;gt; /sys/devices/system/cpu/cpu0/cpufreq/scaling_min_freq", then reboot could be ok. I think reboot command is easy to fix the issue, that I can change the source code to set the higer freq first then execute the reboot sequence. But If the system hangs by other reason, such as other application crash, this solution can not be active. BTW, we can not set CPU freq higher than 800Mhz all the time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 10:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-reboot-hangs-issue/m-p/684974#M105919</guid>
      <dc:creator>caritzhu</dc:creator>
      <dc:date>2017-06-13T10:39:41Z</dc:date>
    </item>
  </channel>
</rss>