<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6: Android: init eth0 with static ip</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684346#M105803</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we are using Android M6.0.1_2.1.0 to a custom hardware with i.mx6dl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to configure eth0 with a static ip address using the Freescale Ethernet App. But after a factory reset this configuration is deleted. We need to add a static ip configuration to system.img.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to do a static ip configuration on default (in system.img)? What it the best way to do it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ludwig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 14:58:57 GMT</pubDate>
    <dc:creator>lzenz</dc:creator>
    <dc:date>2017-07-26T14:58:57Z</dc:date>
    <item>
      <title>imx6: Android: init eth0 with static ip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684346#M105803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we are using Android M6.0.1_2.1.0 to a custom hardware with i.mx6dl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to configure eth0 with a static ip address using the Freescale Ethernet App. But after a factory reset this configuration is deleted. We need to add a static ip configuration to system.img.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to do a static ip configuration on default (in system.img)? What it the best way to do it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ludwig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 14:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684346#M105803</guid>
      <dc:creator>lzenz</dc:creator>
      <dc:date>2017-07-26T14:58:57Z</dc:date>
    </item>
    <item>
      <title>Re: imx6: Android: init eth0 with static ip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684347#M105804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if you used wifi, pls refer to the link as below:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://us.answers.acer.com/app/answers/detail/a_id/11130/~/how-do-i-set-a-static-ip-address-in-the-android-operating-system%3f" title="https://us.answers.acer.com/app/answers/detail/a_id/11130/~/how-do-i-set-a-static-ip-address-in-the-android-operating-system%3f"&gt;How do I set a static IP address in the Android Operating System?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if you use ethernet port, you can use "ifconfig" to set static ip address, like&lt;/P&gt;&lt;P&gt;"ifconfig eth0 &amp;lt;IP ADDRESS&amp;gt;"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 08:01:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684347#M105804</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-08-04T08:01:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx6: Android: init eth0 with static ip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684348#M105805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the infomation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am still not sure how to do it. When I set a static IP with "ifconfig eth0 .... " it works. But when I start the Freescale Ethernet App an run "Check" than it does configure DHCP again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 06:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684348#M105805</guid>
      <dc:creator>lzenz</dc:creator>
      <dc:date>2017-08-09T06:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: imx6: Android: init eth0 with static ip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684349#M105806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can access this from Java space through the console call, pls refer to the link as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/335941"&gt;https://community.nxp.com/thread/335941&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2017 08:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-init-eth0-with-static-ip/m-p/684349#M105806</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-08-10T08:19:01Z</dc:date>
    </item>
  </channel>
</rss>