<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6: Android: save time to /dev/rtc0</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-save-time-to-dev-rtc0/m-p/684327#M105784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we ported Android M6.0.1_2.1.0 to a custom hardware with i.mx6dl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When Android does sync the date and time with the network it is not stored to the /dev/rtc0 device (rtc kernel driver is already working as expected) and is lost when a reboot is done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a mechanism which can be used to store the date and time to /dev/rtc0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ludwig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 14:43:24 GMT</pubDate>
    <dc:creator>lzenz</dc:creator>
    <dc:date>2017-07-26T14:43:24Z</dc:date>
    <item>
      <title>imx6: Android: save time to /dev/rtc0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-save-time-to-dev-rtc0/m-p/684327#M105784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we ported Android M6.0.1_2.1.0 to a custom hardware with i.mx6dl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When Android does sync the date and time with the network it is not stored to the /dev/rtc0 device (rtc kernel driver is already working as expected) and is lost when a reboot is done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a mechanism which can be used to store the date and time to /dev/rtc0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ludwig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 14:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-save-time-to-dev-rtc0/m-p/684327#M105784</guid>
      <dc:creator>lzenz</dc:creator>
      <dc:date>2017-07-26T14:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx6: Android: save time to /dev/rtc0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-save-time-to-dev-rtc0/m-p/684328#M105785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can suggest to add a command to sync the clock into shutdown script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day, &lt;BR /&gt;Victor &lt;BR /&gt; &lt;BR /&gt;----------------------------------------------------------------------------------------------------------------------- &lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you! &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 06:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-save-time-to-dev-rtc0/m-p/684328#M105785</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-07-27T06:14:41Z</dc:date>
    </item>
    <item>
      <title>Re: imx6: Android: save time to /dev/rtc0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-save-time-to-dev-rtc0/m-p/684329#M105786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know a mechanism or hook which does it immediatly after the android system got a valid time from the network?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ludwig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 08:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-Android-save-time-to-dev-rtc0/m-p/684329#M105786</guid>
      <dc:creator>lzenz</dc:creator>
      <dc:date>2017-07-27T08:31:41Z</dc:date>
    </item>
  </channel>
</rss>