<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Interlaced Problem: HD - okay, SD - colour space wrong</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Interlaced-Problem-HD-okay-SD-colour-space-wrong/m-p/684241#M105767</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry Joan, I should have gotten back to this thread sooner. It turns out that our FPGA is treating SD formats differently than HD. Moderators can delete this thread if they want as I don't think it's of any use to anyone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 May 2017 14:02:35 GMT</pubDate>
    <dc:creator>robertspriggs</dc:creator>
    <dc:date>2017-05-24T14:02:35Z</dc:date>
    <item>
      <title>Interlaced Problem: HD - okay, SD - colour space wrong</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interlaced-Problem-HD-okay-SD-colour-space-wrong/m-p/684239#M105765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a custom i.MX6DL board based on the Sabre. I'm using the LDB driver, and our output goes from the IPU display port to an FPGA. I have a number of HD progressive formats working, and I also have these interlaced formats working 1080i50 and 1080i59.94. I have not been able to get either 480i59.94 or 576i50 working. I can get a properly interlaced picture, but the colours are wrong. It looks like I only get luma information, and it's taken incorrectly as chroma, so I see only green and violet, with dark areas of the picture as green and brighter areas as violet. Our FPGA is expecting UYVY16 format. What is different about the SD formats that I need to change?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rob.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT: This is a problem with our hardware, but if anyone needs to use SD formats from &amp;nbsp;the IPU there is a patch here:&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-94019"&gt;https://community.nxp.com/docs/DOC-94019&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 20:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interlaced-Problem-HD-okay-SD-colour-space-wrong/m-p/684239#M105765</guid>
      <dc:creator>robertspriggs</dc:creator>
      <dc:date>2017-05-17T20:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: Interlaced Problem: HD - okay, SD - colour space wrong</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interlaced-Problem-HD-okay-SD-colour-space-wrong/m-p/684240#M105766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what bsp version do you use? and how is your test step? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 May 2017 08:11:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interlaced-Problem-HD-okay-SD-colour-space-wrong/m-p/684240#M105766</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-05-24T08:11:45Z</dc:date>
    </item>
    <item>
      <title>Re: Interlaced Problem: HD - okay, SD - colour space wrong</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interlaced-Problem-HD-okay-SD-colour-space-wrong/m-p/684241#M105767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry Joan, I should have gotten back to this thread sooner. It turns out that our FPGA is treating SD formats differently than HD. Moderators can delete this thread if they want as I don't think it's of any use to anyone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 May 2017 14:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interlaced-Problem-HD-okay-SD-colour-space-wrong/m-p/684241#M105767</guid>
      <dc:creator>robertspriggs</dc:creator>
      <dc:date>2017-05-24T14:02:35Z</dc:date>
    </item>
  </channel>
</rss>