<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX6 - LDB - Display flicker, diagonal print</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683303#M105618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using iMX6DL with Android 5.1.1, Linux kernel 3.14.52. I use LVDS output for display signals. These signals are converted to RGB by an external IC because I use RGB display (only LVDS signals are available from iMX6 hardware).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The display orientation is natively portrait.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The display horizontal lines are increasingly vibrating. At the top, screen is well displayed but at the bottom, horizontal lines are going right to left and left to right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21858i8C75614362A0369D/image-size/large?v=v2&amp;amp;px=999" title="Display Diagonal.JPG" alt="Display Diagonal.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default, display is printed in diagonal. When I turn on "Show layout bounds", vibration stops. At the left of display, some pixels come from de right of the screen.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21901i47B1F04BCCBDC2FE/image-size/large?v=v2&amp;amp;px=999" title="Show layout bounds.JPG" alt="Show layout bounds.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice will help.&lt;BR /&gt;Thanks, Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Jun 2017 09:00:46 GMT</pubDate>
    <dc:creator>pierrelgcb</dc:creator>
    <dc:date>2017-06-12T09:00:46Z</dc:date>
    <item>
      <title>iMX6 - LDB - Display flicker, diagonal print</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683303#M105618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using iMX6DL with Android 5.1.1, Linux kernel 3.14.52. I use LVDS output for display signals. These signals are converted to RGB by an external IC because I use RGB display (only LVDS signals are available from iMX6 hardware).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The display orientation is natively portrait.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The display horizontal lines are increasingly vibrating. At the top, screen is well displayed but at the bottom, horizontal lines are going right to left and left to right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21858i8C75614362A0369D/image-size/large?v=v2&amp;amp;px=999" title="Display Diagonal.JPG" alt="Display Diagonal.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default, display is printed in diagonal. When I turn on "Show layout bounds", vibration stops. At the left of display, some pixels come from de right of the screen.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21901i47B1F04BCCBDC2FE/image-size/large?v=v2&amp;amp;px=999" title="Show layout bounds.JPG" alt="Show layout bounds.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice will help.&lt;BR /&gt;Thanks, Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 09:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683303#M105618</guid>
      <dc:creator>pierrelgcb</dc:creator>
      <dc:date>2017-06-12T09:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 - LDB - Display flicker, diagonal print</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683304#M105619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pierre&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from description seems there is loss of synchronization, this may be due&lt;/P&gt;&lt;P&gt;to incorrect timings from i.MX6 side (for checking one can try to attach true lvds lcd&lt;/P&gt;&lt;P&gt;with similar characteristics) or rgb converter chip. Later may be caused by poor lvds signal,&lt;/P&gt;&lt;P&gt;for example noise, one can try to diminish it by decreasing cable length and fps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 10:29:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683304#M105619</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-12T10:29:51Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 - LDB - Display flicker, diagonal print</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683305#M105620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;Thanks for your advices. I'm working on it. Should takes several days.&lt;/P&gt;&lt;P&gt;Regards, Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 11:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683305#M105620</guid>
      <dc:creator>pierrelgcb</dc:creator>
      <dc:date>2017-06-13T11:01:27Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 - LDB - Display flicker, diagonal print</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683306#M105621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;Problem resolved by hard inverting RGB clock.&lt;/P&gt;&lt;P&gt;Thanks, Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 14:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-LDB-Display-flicker-diagonal-print/m-p/683306#M105621</guid>
      <dc:creator>pierrelgcb</dc:creator>
      <dc:date>2017-06-30T14:05:32Z</dc:date>
    </item>
  </channel>
</rss>