<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックConnect SSP profile bluetooth</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Connect-SSP-profile-bluetooth/m-p/683286#M105607</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I am Working on iMX6ul using Linux. I have to connect device which has SSP profile.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;bluetoothctl controller is used to pair and connect. Pair is done successfully, but it give error when try to connect with device.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;[bluetooth]# connect 00:12:F3:11:A3:80&lt;BR /&gt;Attempting to connect to 00:12:F3:11:A3:80&lt;BR /&gt;[CHG] Device 00:12:F3:11:A3:80 Connected: yes&lt;BR /&gt;Failed to connect: org.bluez.Error.NotAvailable&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;what is the issue with bluetoothctl?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Jignesh&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 05:58:45 GMT</pubDate>
    <dc:creator>jigneshpatel</dc:creator>
    <dc:date>2017-07-26T05:58:45Z</dc:date>
    <item>
      <title>Connect SSP profile bluetooth</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-SSP-profile-bluetooth/m-p/683286#M105607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I am Working on iMX6ul using Linux. I have to connect device which has SSP profile.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;bluetoothctl controller is used to pair and connect. Pair is done successfully, but it give error when try to connect with device.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;[bluetooth]# connect 00:12:F3:11:A3:80&lt;BR /&gt;Attempting to connect to 00:12:F3:11:A3:80&lt;BR /&gt;[CHG] Device 00:12:F3:11:A3:80 Connected: yes&lt;BR /&gt;Failed to connect: org.bluez.Error.NotAvailable&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;what is the issue with bluetoothctl?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Jignesh&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 05:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-SSP-profile-bluetooth/m-p/683286#M105607</guid>
      <dc:creator>jigneshpatel</dc:creator>
      <dc:date>2017-07-26T05:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: Connect SSP profile bluetooth</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-SSP-profile-bluetooth/m-p/683287#M105608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Jignesh&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;current bsp package supports BlueZ 5.28 and one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://stackoverflow.com/questions/26950002/how-do-i-get-bluez-5-to-accept-a-fixed-pin"&gt;https://stackoverflow.com/questions/26950002/how-do-i-get-bluez-5-to-accept-a-fixed-pin&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 23:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-SSP-profile-bluetooth/m-p/683287#M105608</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-26T23:23:54Z</dc:date>
    </item>
  </channel>
</rss>