<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Does imx6ul linux use OCRAM?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-imx6ul-linux-use-OCRAM/m-p/682720#M105505</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Charlie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes uses (seems one can use linker map for that), for example&lt;/P&gt;&lt;P&gt;low power driver, described in attached Linux Manual Chapter 21&lt;BR /&gt;Low-level Power Management (PM) Driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 May 2017 23:04:29 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-05-17T23:04:29Z</dc:date>
    <item>
      <title>Does imx6ul linux use OCRAM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-imx6ul-linux-use-OCRAM/m-p/682719#M105504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The imx6ul RM says it uses some OCRAM during boot, but after that it is free. Does imx6ul linux use OCRAM? In looking at pm-imx6.c, it is not clear to me with respect to the ul version of the imx6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 19:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-imx6ul-linux-use-OCRAM/m-p/682719#M105504</guid>
      <dc:creator>charlieschultz</dc:creator>
      <dc:date>2017-05-17T19:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: Does imx6ul linux use OCRAM?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-imx6ul-linux-use-OCRAM/m-p/682720#M105505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Charlie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes uses (seems one can use linker map for that), for example&lt;/P&gt;&lt;P&gt;low power driver, described in attached Linux Manual Chapter 21&lt;BR /&gt;Low-level Power Management (PM) Driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 23:04:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-imx6ul-linux-use-OCRAM/m-p/682720#M105505</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-17T23:04:29Z</dc:date>
    </item>
  </channel>
</rss>