<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Inflexion 2.4 Update Now Available in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197143#M10545</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Phil. That explains. Only&amp;nbsp;tried it on the single WVGA LCD so did not notice the High resolution support included. Will&amp;nbsp;try and transfer&amp;nbsp;my project&amp;nbsp;to 2.4 soon.&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Dec 2011 15:56:31 GMT</pubDate>
    <dc:creator>xizhouwang</dc:creator>
    <dc:date>2011-12-20T15:56:31Z</dc:date>
    <item>
      <title>Inflexion 2.4 Update Now Available</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197140#M10542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are pleased to announce that a new release of the award winning Mentor Embedded Inflexion UI for i.MX processors is now available for download.&lt;/P&gt;&lt;P&gt;The release contains a number of enhancements, including runtime performance improvements, usability improvements, bug fixes, support for the i.MX53 SABRE and a complete re-write of the Linux getting started guide. This makes it even easier to transform your product with compelling and dynamic UIs.&lt;/P&gt;&lt;P&gt;Visit the below link to download the new release now:&lt;/P&gt;&lt;P&gt;&lt;A href="http://go.mentor.com/imxinflexion"&gt;http://go.mentor.com/imxinflexion&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 11:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197140#M10542</guid>
      <dc:creator>PhilBrumby</dc:creator>
      <dc:date>2011-12-20T11:05:32Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion 2.4 Update Now Available</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197141#M10543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Recompiled the inflexionui_demo on the new 2.4, the excutable size is 7.8MB while from the vrsion 2.3&amp;nbsp;it was 5.1MB for&amp;nbsp;i.MX53 QSB running Linux 1109 BSP with GLE lib. Thanks for the PDF document update.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 14:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197141#M10543</guid>
      <dc:creator>xizhouwang</dc:creator>
      <dc:date>2011-12-20T14:37:35Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion 2.4 Update Now Available</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197142#M10544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The default demo has increased significantly in size because it now supports HD (720p &amp;amp; 1080p) as an output.&lt;/P&gt;&lt;P&gt;This generic demo supports multiple resolutions and so makes use of multiple sized versions of resources that increase the size of the theme. A standard app would not do this, it is only for ease of demo purpose over multiple resolutions.&lt;/P&gt;&lt;P&gt;The Runtime Engine itself has had a minimal footprint size increase of ~100Kb for this 2.4 release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Phil.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 14:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197142#M10544</guid>
      <dc:creator>PhilBrumby</dc:creator>
      <dc:date>2011-12-20T14:55:55Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion 2.4 Update Now Available</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197143#M10545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Phil. That explains. Only&amp;nbsp;tried it on the single WVGA LCD so did not notice the High resolution support included. Will&amp;nbsp;try and transfer&amp;nbsp;my project&amp;nbsp;to 2.4 soon.&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 15:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-2-4-Update-Now-Available/m-p/197143#M10545</guid>
      <dc:creator>xizhouwang</dc:creator>
      <dc:date>2011-12-20T15:56:31Z</dc:date>
    </item>
  </channel>
</rss>