<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flexcan transceiver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flexcan-transceiver/m-p/682390#M105439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kishore&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for testing one can use unit tests (imx-test), check folder ..test/can/&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;please refer to Chapter 37 FlexCAN Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Jul 2017 23:49:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-07-25T23:49:55Z</dc:date>
    <item>
      <title>Flexcan transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flexcan-transceiver/m-p/682389#M105438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to IMX platform devices. I have IMX6 sabrelite board with flexcan controller embedded on it.&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i able to communicate with that from userspace i think i need flexcan transceiver also to communicate with flexcan controller so is there any transceiver on IMX6 board itself or i need to mount ??&lt;/P&gt;&lt;P&gt;What are the transceivers are supported by flexcan controller and is there any software drivers are required for that.&lt;/P&gt;&lt;P&gt;Can you please clarify these .&lt;/P&gt;&lt;P&gt;thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2017 14:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flexcan-transceiver/m-p/682389#M105438</guid>
      <dc:creator>kishorekrish</dc:creator>
      <dc:date>2017-07-25T14:12:35Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcan transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flexcan-transceiver/m-p/682390#M105439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kishore&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for testing one can use unit tests (imx-test), check folder ..test/can/&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;please refer to Chapter 37 FlexCAN Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2017 23:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flexcan-transceiver/m-p/682390#M105439</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-25T23:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcan transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flexcan-transceiver/m-p/682391#M105440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;Thanks for ur reply.&lt;/P&gt;&lt;P&gt;Actually this testing was already done by someone.&lt;/P&gt;&lt;P&gt;i want to understand in real time how this controller and transceiver will work??&lt;/P&gt;&lt;P&gt;If i want to send any data from application level it has to gothrough TCP/IP stack and then .ndo_start_xmit of controller driver call back will triggered, this is right or wrong??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is correct what is my maximum buffer size i can transmit using CAN bus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Kishore.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 06:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flexcan-transceiver/m-p/682391#M105440</guid>
      <dc:creator>kishorekrish</dc:creator>
      <dc:date>2017-07-28T06:41:54Z</dc:date>
    </item>
  </channel>
</rss>