<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PF3000 PMIC 5V powered</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF3000-PMIC-5V-powered/m-p/682204#M105408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for 5V fet should be used according to Table 2. Pin definitions, also&lt;BR /&gt;VLDO inputs are not connected to VIN/VPWR by default&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fanalog%2Fdoc%2Fdata_sheet%2FPF3000.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/PF3000.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 11 Jun 2017 22:59:15 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-06-11T22:59:15Z</dc:date>
    <item>
      <title>PF3000 PMIC 5V powered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF3000-PMIC-5V-powered/m-p/682203#M105407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I want to use a pf3000 pmic on my imx6ul design. It will not be battery backed up. V supply will be 5V, so that means I will be using the VPWR input pin. In all reference designs I have come across, the VIN pin (&amp;lt;4.5V) is also used, and a FET is used to switch between inputs. I presume I can leave this FET out?&lt;/P&gt;&lt;P&gt;Also I notice on reference designs, the SW and LDO regs are tied to the &amp;lt;4.5V source. Are the inputs to these regulators not connected to the VIN/VPWR pin already?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 15:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF3000-PMIC-5V-powered/m-p/682203#M105407</guid>
      <dc:creator>patrickoreilly</dc:creator>
      <dc:date>2017-06-09T15:51:44Z</dc:date>
    </item>
    <item>
      <title>Re: PF3000 PMIC 5V powered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF3000-PMIC-5V-powered/m-p/682204#M105408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for 5V fet should be used according to Table 2. Pin definitions, also&lt;BR /&gt;VLDO inputs are not connected to VIN/VPWR by default&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fanalog%2Fdoc%2Fdata_sheet%2FPF3000.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/PF3000.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Jun 2017 22:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF3000-PMIC-5V-powered/m-p/682204#M105408</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-11T22:59:15Z</dc:date>
    </item>
  </channel>
</rss>