<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ERROR: do_preconfigure issue in Yocto Krogoth (Kernel 4.1.15) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-do-preconfigure-issue-in-Yocto-Krogoth-Kernel-4-1-15/m-p/682004#M105365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anuradha Ranasinghe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The menuconfig error may be related to the shell not being able to show the menuconfig window correctly. This may happen if you are using the shell from a simple terminal or from a window that is too small.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m not so familiar with Boundary Device’s kernel but maybe&amp;nbsp; &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/gary_bisson"&gt;gary_bisson&lt;/A&gt;may be able to give us some suggestions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Jul 2017 16:35:45 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-07-05T16:35:45Z</dc:date>
    <item>
      <title>ERROR: do_preconfigure issue in Yocto Krogoth (Kernel 4.1.15)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-do-preconfigure-issue-in-Yocto-Krogoth-Kernel-4-1-15/m-p/682003#M105364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #555555; background-color: #ffffff; font-size: 16px; margin: 0px 0px 1.313em;"&gt;Hi All,&lt;/P&gt;&lt;P style="color: #555555; background-color: #ffffff; font-size: 16px; margin: 0px 0px 1.313em;"&gt;I am using Krogoth version with Boundary Devices kernel 4.1.15. After cleansstate of core-image-minimal, now I cannot run :&lt;BR /&gt;&amp;gt; bitbake linux-boundary -c menuconfig&lt;BR /&gt;&amp;gt; bitbake linux-boundary -c compile -f&lt;BR /&gt;or any other bitbake commands. I can see following error message in the terminal :&lt;/P&gt;&lt;P style="color: #555555; background-color: #ffffff; font-size: 16px; margin: 0px 0px 1.313em;"&gt;Terminal Output :&lt;/P&gt;&lt;P style="color: #555555; background-color: #ffffff; font-size: 16px; margin: 0px 0px 1.313em;"&gt;ERROR: linux-boundary-4.1.15-r0 do_preconfigure: Function failed: do_preconfigure (log file is located at /home/tengri/Desktop/krogoth/core-image-minimal/tmp/work/nitrogen6x-poky-linux-gnueabi/linux-boundary/4.1.15-r0/temp/log.do_preconfigure.6371)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/tengri/Desktop/krogoth/core-image-minimal/tmp/work/nitrogen6x-poky-linux-gnueabi/linux-boundary/4.1.15-r0/temp/log.do_preconfigure.6371&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_preconfigure&lt;BR /&gt;| WARNING: exit code 128 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_preconfigure (log file is located at /home/tengri/Desktop/krogoth/core-image-minimal/tmp/work/nitrogen6x-poky-linux-gnueabi/linux-boundary/4.1.15-r0/temp/log.do_preconfigure.6371)&lt;BR /&gt;ERROR: Task 3 (/home/tengri/Desktop/krogoth/sources/meta-fsl-arm-extra/recipes-kernel/linux/linux-boundary_4.1.15.bb, do_preconfigure) failed with exit code ‘1’&lt;BR /&gt;NOTE: Tasks Summary: Attempted 250 tasks of which 249 didn’t need to be rerun and 1 failed.&lt;BR /&gt;No currently running tasks (250 of 252)&lt;/P&gt;&lt;P style="color: #555555; background-color: #ffffff; font-size: 16px;"&gt;Can anyone give me an insight to solve this issue ?&lt;/P&gt;&lt;P style="color: #555555; background-color: #ffffff; font-size: 16px;"&gt;Thanks in Advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jul 2017 11:15:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-do-preconfigure-issue-in-Yocto-Krogoth-Kernel-4-1-15/m-p/682003#M105364</guid>
      <dc:creator>tengri</dc:creator>
      <dc:date>2017-07-03T11:15:56Z</dc:date>
    </item>
    <item>
      <title>Re: ERROR: do_preconfigure issue in Yocto Krogoth (Kernel 4.1.15)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-do-preconfigure-issue-in-Yocto-Krogoth-Kernel-4-1-15/m-p/682004#M105365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anuradha Ranasinghe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The menuconfig error may be related to the shell not being able to show the menuconfig window correctly. This may happen if you are using the shell from a simple terminal or from a window that is too small.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m not so familiar with Boundary Device’s kernel but maybe&amp;nbsp; &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/gary_bisson"&gt;gary_bisson&lt;/A&gt;may be able to give us some suggestions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2017 16:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-do-preconfigure-issue-in-Yocto-Krogoth-Kernel-4-1-15/m-p/682004#M105365</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-07-05T16:35:45Z</dc:date>
    </item>
    <item>
      <title>Re: ERROR: do_preconfigure issue in Yocto Krogoth (Kernel 4.1.15)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-do-preconfigure-issue-in-Yocto-Krogoth-Kernel-4-1-15/m-p/682005#M105366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've replied to&amp;nbsp;Anuradha on our website that we need to see the log.preconfigure in order to understand what is going on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But note that Boundary Devices kernel is based upon NXP one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, after trying those commands here it worked fine, even the menuconfig, so I suspect a setup issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2017 16:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-do-preconfigure-issue-in-Yocto-Krogoth-Kernel-4-1-15/m-p/682005#M105366</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2017-07-05T16:52:03Z</dc:date>
    </item>
  </channel>
</rss>