<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX7 eMMC and NAND at the same time in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eMMC-and-NAND-at-the-same-time/m-p/681075#M105206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently planning a hardware design using an i.MX7. Our customer would like to use both NAND and eMMC flash (to strictly split boot and data files).&lt;/P&gt;&lt;P&gt;The plan was to use SD3/SAI1 in alternate pin mux 1 to provide the NAND interface and SD1 to connect to the eMMC.&lt;/P&gt;&lt;P&gt;However, SD1 seems to not have a strobe signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use both eMMC (v5) and NAND&amp;nbsp;at the same time?&lt;BR /&gt;(From what i have seen, the strobe signal is only used in HS400 mode. In this case, i could use any eMMC in HS200 mode?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Jul 2017 14:40:37 GMT</pubDate>
    <dc:creator>demoniacmilk</dc:creator>
    <dc:date>2017-07-03T14:40:37Z</dc:date>
    <item>
      <title>i.MX7 eMMC and NAND at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eMMC-and-NAND-at-the-same-time/m-p/681075#M105206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently planning a hardware design using an i.MX7. Our customer would like to use both NAND and eMMC flash (to strictly split boot and data files).&lt;/P&gt;&lt;P&gt;The plan was to use SD3/SAI1 in alternate pin mux 1 to provide the NAND interface and SD1 to connect to the eMMC.&lt;/P&gt;&lt;P&gt;However, SD1 seems to not have a strobe signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use both eMMC (v5) and NAND&amp;nbsp;at the same time?&lt;BR /&gt;(From what i have seen, the strobe signal is only used in HS400 mode. In this case, i could use any eMMC in HS200 mode?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jul 2017 14:40:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eMMC-and-NAND-at-the-same-time/m-p/681075#M105206</guid>
      <dc:creator>demoniacmilk</dc:creator>
      <dc:date>2017-07-03T14:40:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 eMMC and NAND at the same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eMMC-and-NAND-at-the-same-time/m-p/681076#M105207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, strobe signal is optional signal used in HS400 mode.&lt;/P&gt;&lt;P&gt;One can use any eMMC in other modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jul 2017 23:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eMMC-and-NAND-at-the-same-time/m-p/681076#M105207</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-03T23:39:51Z</dc:date>
    </item>
  </channel>
</rss>