<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6UL USB OTG in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-USB-OTG/m-p/680793#M105157</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;per usb specification ID signal should be high (or float) in Device mode,&lt;/P&gt;&lt;P&gt;low in Host. It is used by linux driver,&amp;nbsp; I am afraid it is not possible to set it by software&lt;/P&gt;&lt;P&gt;without additional modifications in linux sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2017 23:20:21 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-07-24T23:20:21Z</dc:date>
    <item>
      <title>i.MX6UL USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-USB-OTG/m-p/680791#M105155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question regarding the USB OTG interface on the IMX6UL. I am using the i.MX6UL in a custom Hardware Design and I am wondering if it is neccessary to set the ID Signal High or Low by external Components. I need a lot of Interfaces and Analog Inputs, so the muxed Pins ID, OC and PWR are blocked by other functions. &lt;/P&gt;&lt;P&gt;Is it possible to set these by Software?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 11:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-USB-OTG/m-p/680791#M105155</guid>
      <dc:creator>martinwerner</dc:creator>
      <dc:date>2017-07-24T11:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-USB-OTG/m-p/680792#M105156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;BTW: I want to use the i.MX6 as USB Host.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 12:03:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-USB-OTG/m-p/680792#M105156</guid>
      <dc:creator>martinwerner</dc:creator>
      <dc:date>2017-07-24T12:03:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-USB-OTG/m-p/680793#M105157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;per usb specification ID signal should be high (or float) in Device mode,&lt;/P&gt;&lt;P&gt;low in Host. It is used by linux driver,&amp;nbsp; I am afraid it is not possible to set it by software&lt;/P&gt;&lt;P&gt;without additional modifications in linux sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 23:20:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-USB-OTG/m-p/680793#M105157</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-24T23:20:21Z</dc:date>
    </item>
  </channel>
</rss>