<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Enabling MIPI DSI interface on freescale Yocto build in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-MIPI-DSI-interface-on-freescale-Yocto-build/m-p/680400#M105086</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What are the steps to enable and configure MIPI DSI on freescale's yocto platform? I'm using a Variscite iMX.6 board and have been developing with the LVDS interface. Connecting a TFT to the MIPI DSI is giving me nothing, and I'm struggling to find documentation for;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Is the MIPI DSI enabled in the kernel? Is there a driver?&lt;/P&gt;&lt;P&gt;- If so... What config files do I create or enable, to configure the interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 May 2017 20:43:18 GMT</pubDate>
    <dc:creator>epicedium</dc:creator>
    <dc:date>2017-05-15T20:43:18Z</dc:date>
    <item>
      <title>Enabling MIPI DSI interface on freescale Yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-MIPI-DSI-interface-on-freescale-Yocto-build/m-p/680400#M105086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What are the steps to enable and configure MIPI DSI on freescale's yocto platform? I'm using a Variscite iMX.6 board and have been developing with the LVDS interface. Connecting a TFT to the MIPI DSI is giving me nothing, and I'm struggling to find documentation for;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Is the MIPI DSI enabled in the kernel? Is there a driver?&lt;/P&gt;&lt;P&gt;- If so... What config files do I create or enable, to configure the interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 20:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-MIPI-DSI-interface-on-freescale-Yocto-build/m-p/680400#M105086</guid>
      <dc:creator>epicedium</dc:creator>
      <dc:date>2017-05-15T20:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling MIPI DSI interface on freescale Yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-MIPI-DSI-interface-on-freescale-Yocto-build/m-p/680401#M105087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to Linux documentation (Linux Manual, MIPI DSI Chapter ) on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 23:25:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-MIPI-DSI-interface-on-freescale-Yocto-build/m-p/680401#M105087</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-15T23:25:10Z</dc:date>
    </item>
  </channel>
</rss>