<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Scrolling video MIPI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Scrolling-video-MIPI/m-p/680253#M105062</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;did you see the interrupt when video scrolling? and try to check if your VSYNC and HSYNC are correct or not, I'm not sure what do you set them,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 10:02:59 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2017-07-26T10:02:59Z</dc:date>
    <item>
      <title>Scrolling video MIPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Scrolling-video-MIPI/m-p/680252#M105061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have successfully interfaced my MIPI camera (Sony MA130) but I have a strange behavior.&lt;/P&gt;&lt;P&gt;When I power up the board and start the pipeline, everything works fine.&lt;/P&gt;&lt;P&gt;When I stop and restart the pipeline (without restarting the board) I have the following warning :&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001&lt;/P&gt;&lt;P&gt;And the video is scrolling down until reaching the correct position.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the documentation this register means :&lt;/P&gt;&lt;P&gt;Frame Lost of SMFC channel 0 interrupt.&lt;BR /&gt;This bit indicates on an interrupt that is a result of a result of a Frame Lost of SMFC channel 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to modify lot of registers but I can't find the source of my issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Pierre-Olivier Huard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 09:07:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Scrolling-video-MIPI/m-p/680252#M105061</guid>
      <dc:creator>pierre-olivierh</dc:creator>
      <dc:date>2017-07-24T09:07:21Z</dc:date>
    </item>
    <item>
      <title>Re: Scrolling video MIPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Scrolling-video-MIPI/m-p/680253#M105062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;did you see the interrupt when video scrolling? and try to check if your VSYNC and HSYNC are correct or not, I'm not sure what do you set them,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 10:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Scrolling-video-MIPI/m-p/680253#M105062</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-07-26T10:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: Scrolling video MIPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Scrolling-video-MIPI/m-p/680254#M105063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The IPU warning occurs when I start the gstreamer pipeline. It does not occurs during the video.&lt;/P&gt;&lt;P&gt;This is my registers:&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 185.121846] IPU ID = 0, CSI ID = 0&lt;BR /&gt;[&amp;nbsp; 185.125253] IPU_CONF = 0x10000761&lt;BR /&gt;[&amp;nbsp; 185.128571] CSI_SENS_CONF = 0x00008A10&lt;BR /&gt;[&amp;nbsp; 185.132355] CSI_SENS_FRM_SIZE = 0x02CF04FF&lt;BR /&gt;[&amp;nbsp; 185.136462] CSI_ACT_FRM_SIZE = 0x02CF04FF&lt;BR /&gt;[&amp;nbsp; 185.140548] CSI_OUT_FRM_CTRL = 0x00000000&lt;BR /&gt;[&amp;nbsp; 185.144564] CSI_TST_CTRL = 0x00000000&lt;BR /&gt;[&amp;nbsp; 185.148231] CSI_CCIR_CODE_1 = 0x00040030&lt;BR /&gt;[&amp;nbsp; 185.152183] CSI_CCIR_CODE_2 = 0x00000000&lt;BR /&gt;[&amp;nbsp; 185.156118] CSI_CCIR_CODE_3 = 0x00FF0000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MIPI is 2 lanes, 648MHz DDR clock. VC=0, IPU10 CSI0&lt;/P&gt;&lt;P&gt;The Format is YCbCr (YUV422)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I check the Vsync Hsync? It's embedded in the MIPI lanes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 09:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Scrolling-video-MIPI/m-p/680254#M105063</guid>
      <dc:creator>pierre-olivierh</dc:creator>
      <dc:date>2017-07-28T09:02:36Z</dc:date>
    </item>
  </channel>
</rss>