<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX53 Build for SMD (Sabre) Tablet in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-Build-for-SMD-Sabre-Tablet/m-p/196734#M10505</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi - I've got a working X11 build for the Sabre tablet, and I have a working OpenGL environment. When I build the IMX53 GPU samples from the GPU SDK, they run very slowly on the Sabre target (approx. 5-7 FPS for the pinball example). When I run the run the pre-installed examples in the Linux BSP for the Quick Start board, the performance is much better (approx. 27-33 FPS for the pinball example).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Any ideas for the significant difference in performance?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Dec 2011 21:59:26 GMT</pubDate>
    <dc:creator>MichaelGale</dc:creator>
    <dc:date>2011-12-19T21:59:26Z</dc:date>
    <item>
      <title>IMX53 Build for SMD (Sabre) Tablet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX53-Build-for-SMD-Sabre-Tablet/m-p/196734#M10505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi - I've got a working X11 build for the Sabre tablet, and I have a working OpenGL environment. When I build the IMX53 GPU samples from the GPU SDK, they run very slowly on the Sabre target (approx. 5-7 FPS for the pinball example). When I run the run the pre-installed examples in the Linux BSP for the Quick Start board, the performance is much better (approx. 27-33 FPS for the pinball example).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Any ideas for the significant difference in performance?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2011 21:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX53-Build-for-SMD-Sabre-Tablet/m-p/196734#M10505</guid>
      <dc:creator>MichaelGale</dc:creator>
      <dc:date>2011-12-19T21:59:26Z</dc:date>
    </item>
  </channel>
</rss>