<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: qt compositor</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/qt-compositor/m-p/680060#M105009</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;in hope of some one find it useful,&lt;/P&gt;&lt;P&gt;i built &lt;EM&gt;"fsl-image-gui" &amp;nbsp;&lt;/EM&gt;(i added qtwayland in the local.conf, IMAGE_INSTALL)&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;on this image then i copied the content of qtwayland/image/usr to the rootfs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;i was able to run qtcompositor.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;the difference is this time i have "&lt;EM&gt;eglfs&lt;/EM&gt;" platform and i used &lt;STRONG&gt;--platform eglfs&lt;/STRONG&gt; to run qtcompositor. i thought wayland compositors are able to be run with all ather backends even wayland itself. but i couldn't do it. &lt;STRONG&gt;it works just with eglfs.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i wish someone could tell me how to add &lt;EM&gt;eglfs&lt;/EM&gt; to &lt;EM&gt;"fsl-image-qt5&lt;/EM&gt;"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;i added :&amp;nbsp;&lt;/P&gt;&lt;P&gt;PACKAGECONFIG_DISTRO_pn-qtbase+=" eglfs "&lt;/P&gt;&lt;P&gt;but the image still does not have eglfs and i hve to use "&lt;EM&gt;fsl-image-qt5&lt;/EM&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;good luck everybody&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 04:41:29 GMT</pubDate>
    <dc:creator>adelantesey</dc:creator>
    <dc:date>2017-07-26T04:41:29Z</dc:date>
    <item>
      <title>qt compositor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qt-compositor/m-p/680059#M105008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I have imx6sxsabresd, yocto 4.1.0-2.1.0 from NXP.&lt;/P&gt;&lt;P&gt;i built image &lt;STRONG&gt;fsl-image-qt5&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;also &lt;STRONG&gt;qtwayland&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;weston works fine.&lt;/P&gt;&lt;P&gt;qml-compositor example does not work:&lt;/P&gt;&lt;P&gt;on running weston :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;unable to lock lockfile /run/user/root/wayland-0.lock, maybe another compositor is running.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;without weston:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;QXcbConnection: Could not connect to display : 0.0&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS:&lt;/P&gt;&lt;P&gt;LD_LIBRARY_PATH=/usr/lib&lt;/P&gt;&lt;P&gt;DISPLAY=:0.0&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for qtwayland i copied :&lt;/P&gt;&lt;P&gt;&amp;lt;board dir&amp;gt;/tmp/work/cortexA9hf-neon-mx6sx-poky-linux-gnueabi/qtwayland/image/usr &lt;STRONG&gt;to&lt;/STRONG&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&amp;lt;board&amp;gt;/usr/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could anyone help me please?&lt;/P&gt;&lt;P&gt;1- should i bitbake another image?&lt;/P&gt;&lt;P&gt;2- should i compile compositor and install it on board?&lt;/P&gt;&lt;P&gt;3- do i need specific environment variable?&amp;nbsp;&lt;/P&gt;&lt;P&gt;4- does qtwayland works for this distribution i have?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Jul 2017 11:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qt-compositor/m-p/680059#M105008</guid>
      <dc:creator>adelantesey</dc:creator>
      <dc:date>2017-07-22T11:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: qt compositor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qt-compositor/m-p/680060#M105009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;in hope of some one find it useful,&lt;/P&gt;&lt;P&gt;i built &lt;EM&gt;"fsl-image-gui" &amp;nbsp;&lt;/EM&gt;(i added qtwayland in the local.conf, IMAGE_INSTALL)&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;on this image then i copied the content of qtwayland/image/usr to the rootfs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;i was able to run qtcompositor.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;the difference is this time i have "&lt;EM&gt;eglfs&lt;/EM&gt;" platform and i used &lt;STRONG&gt;--platform eglfs&lt;/STRONG&gt; to run qtcompositor. i thought wayland compositors are able to be run with all ather backends even wayland itself. but i couldn't do it. &lt;STRONG&gt;it works just with eglfs.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i wish someone could tell me how to add &lt;EM&gt;eglfs&lt;/EM&gt; to &lt;EM&gt;"fsl-image-qt5&lt;/EM&gt;"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;i added :&amp;nbsp;&lt;/P&gt;&lt;P&gt;PACKAGECONFIG_DISTRO_pn-qtbase+=" eglfs "&lt;/P&gt;&lt;P&gt;but the image still does not have eglfs and i hve to use "&lt;EM&gt;fsl-image-qt5&lt;/EM&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;good luck everybody&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 04:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qt-compositor/m-p/680060#M105009</guid>
      <dc:creator>adelantesey</dc:creator>
      <dc:date>2017-07-26T04:41:29Z</dc:date>
    </item>
  </channel>
</rss>