<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Imx6q fec dump</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Imx6q-fec-dump/m-p/679741#M104951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jacky&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check fec configuration using Chapter 37&lt;BR /&gt;Fast Ethernet Controller (FEC) Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;Also exception can be caused by ddr errors, may be recommended to run&lt;/P&gt;&lt;P&gt;ddr test and rebuild image with new calibration coefficients.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Jun 2017 06:17:39 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-06-08T06:17:39Z</dc:date>
    <item>
      <title>Imx6q fec dump</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6q-fec-dump/m-p/679740#M104950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,everyone:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I am working on a imx6q board with linux-3.0.35,and i have issue. In kernel source there is no fec.c but a fec.module instead in /driver/net/ .and the kernel &amp;nbsp;stoped &amp;nbsp;after fec_enet_mii_bus: probed&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 2.276373] Fixed MDIO Bus: probed&lt;BR /&gt;[ 2.280383] vcan: Virtual CAN interface driver&lt;BR /&gt;[ 2.284832] CAN device driver interface&lt;BR /&gt;[ 2.288672] flexcan netdevice driver&lt;BR /&gt;[ 2.292398] FEC Ethernet Driver&lt;BR /&gt;[ 2.297699] fec_enet_mii_bus: probed&lt;BR /&gt;[ 2.301323] Unable to handle kernel NULL pointer dereference at virtual address 00000000&lt;BR /&gt;[ 2.309422] pgd = 80004000&lt;BR /&gt;[ 2.312151] [00000000] *pgd=00000000&lt;BR /&gt;[ 2.315745] Internal error: Oops: 5 [#1] PREEMPT SMP&lt;BR /&gt;[ 2.320713] Modules linked in:&lt;BR /&gt;[ 2.323785] CPU: 0 Not tainted (3.0.35-2508-g54750ff #106)&lt;BR /&gt;[ 2.329635] PC is at register_netdevice+0x5c/0x37c&lt;BR /&gt;[ 2.334431] LR is at 0x30687465&lt;BR /&gt;[ 2.337576] pc : [&amp;lt;80345190&amp;gt;] lr : [&amp;lt;30687465&amp;gt;] psr: 60000013&lt;BR /&gt;[ 2.337581] sp : e9fddeb0 ip : 0000001c fp : fffffffa&lt;BR /&gt;[ 2.349070] r10: e4405400 r9 : e9e91808 r8 : e9e88e60&lt;BR /&gt;[ 2.354297] r7 : e4455460 r6 : e9afc000 r5 : 00000000 r4 : e9afc000&lt;BR /&gt;[ 2.360827] r3 : 00000000 r2 : 00000000 r1 : e9fdde80 r0 : 00000000&lt;BR /&gt;[ 2.367359] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel&lt;BR /&gt;[ 2.374672] Control: 10c53c7d Table: 1000404a DAC: 00000015&lt;BR /&gt;[ 2.380419] Process swapper (pid: 1, stack limit = 0xe9fdc2f0)&lt;BR /&gt;[ 2.386256] Stack: (0xe9fddeb0 to 0xe9fde000)&lt;BR /&gt;[ 2.390620] dea0: e9afc000 e9e91800 e9afc000 e4455460&lt;BR /&gt;[ 2.398803] dec0: e9e88e60 803454c4 e9afc000 803fd268 e9e91968 e9afc000 e9fcbed8 805a9c90&lt;BR /&gt;[ 2.406986] dee0: e9e8f398 00000000 e9e91808 e9e91808 805f2b28 e9e9183c 00000000 805a9b7c&lt;BR /&gt;[ 2.415169] df00: 00000000 8001e2fc 00000000 8027e2f4 8027e2dc 8027d128 e9e91808 805a9b7c&lt;BR /&gt;[ 2.423351] df20: e9e9183c 00000000 00000000 8027d2c0 805a9b7c 00000000 8027d234 8027c364&lt;BR /&gt;[ 2.431534] df40: e9f06c00 e9e8bb38 805a9b7c 805a75c8 e44496c0 8027cb04 804d6668 805a9b7c&lt;BR /&gt;[ 2.439716] df60: e9fdc000 805a9b7c e9fdc000 80038ad8 00000000 00000000 8001e2fc 8027d76c&lt;BR /&gt;[ 2.447899] df80: 805bc540 e9fdc000 80038ad8 00000000 00000000 8003253c 800a9014 8057d080&lt;BR /&gt;[ 2.456082] dfa0: 000001df 8001e2fc 000001df 00000013 00000000 3734ea08 00000039 00000000&lt;BR /&gt;[ 2.464264] dfc0: 80592aa8 80029238 80029370 80038ad8 00000013 00000000 00000000 00000000&lt;BR /&gt;[ 2.472446] dfe0: 00000000 800089ac 00000000 00000000 80008914 80038ad8 fdd7fabe fffbdf5e&lt;BR /&gt;[ 2.480642] [&amp;lt;80345190&amp;gt;] (register_netdevice+0x5c/0x37c) from [&amp;lt;803454c4&amp;gt;] (register_netdev+0x14/0x24)&lt;BR /&gt;[ 2.489963] [&amp;lt;803454c4&amp;gt;] (register_netdev+0x14/0x24) from [&amp;lt;803fd268&amp;gt;] (fec_probe+0x6f0/0x748)&lt;BR /&gt;[ 2.498595] [&amp;lt;803fd268&amp;gt;] (fec_probe+0x6f0/0x748) from [&amp;lt;8027e2f4&amp;gt;] (platform_drv_probe+0x18/0x1c)&lt;BR /&gt;[ 2.507481] [&amp;lt;8027e2f4&amp;gt;] (platform_drv_probe+0x18/0x1c) from [&amp;lt;8027d128&amp;gt;] (driver_probe_device+0x90/0x19c)&lt;BR /&gt;[ 2.517144] [&amp;lt;8027d128&amp;gt;] (driver_probe_device+0x90/0x19c) from [&amp;lt;8027d2c0&amp;gt;] (__driver_attach+0x8c/0x90)&lt;BR /&gt;[ 2.526547] [&amp;lt;8027d2c0&amp;gt;] (__driver_attach+0x8c/0x90) from [&amp;lt;8027c364&amp;gt;] (bus_for_each_dev+0x5c/0x88)&lt;BR /&gt;[ 2.535602] [&amp;lt;8027c364&amp;gt;] (bus_for_each_dev+0x5c/0x88) from [&amp;lt;8027cb04&amp;gt;] (bus_add_driver+0x178/0x238)&lt;BR /&gt;[ 2.544743] [&amp;lt;8027cb04&amp;gt;] (bus_add_driver+0x178/0x238) from [&amp;lt;8027d76c&amp;gt;] (driver_register+0x78/0x13c)&lt;BR /&gt;[ 2.553896] [&amp;lt;8027d76c&amp;gt;] (driver_register+0x78/0x13c) from [&amp;lt;8003253c&amp;gt;] (do_one_initcall+0x34/0x174)&lt;BR /&gt;[ 2.563041] [&amp;lt;8003253c&amp;gt;] (do_one_initcall+0x34/0x174) from [&amp;lt;800089ac&amp;gt;] (kernel_init+0x98/0x13c)&lt;BR /&gt;[ 2.571842] [&amp;lt;800089ac&amp;gt;] (kernel_init+0x98/0x13c) from [&amp;lt;80038ad8&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;BR /&gt;[ 2.580635] Code: e1a06004 e2505000 ba000042 e59430d8 (e5933000) &lt;BR /&gt;[ 2.586762] ---[ end trace 99a6ae3ba28139d5 ]---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how could i solv this problem? thanks very much!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 03:44:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6q-fec-dump/m-p/679740#M104950</guid>
      <dc:creator>Jacky_Song</dc:creator>
      <dc:date>2017-06-08T03:44:20Z</dc:date>
    </item>
    <item>
      <title>Re: Imx6q fec dump</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6q-fec-dump/m-p/679741#M104951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jacky&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check fec configuration using Chapter 37&lt;BR /&gt;Fast Ethernet Controller (FEC) Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;Also exception can be caused by ddr errors, may be recommended to run&lt;/P&gt;&lt;P&gt;ddr test and rebuild image with new calibration coefficients.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 06:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6q-fec-dump/m-p/679741#M104951</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-06-08T06:17:39Z</dc:date>
    </item>
    <item>
      <title>Re: Imx6q fec dump</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6q-fec-dump/m-p/679742#M104952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,i'm sorry for no reply&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the fec is ok now. the configure has problem,when i choose ppp driver and wireless hostapd the kernel goes well.and i dont kown why. anyway it's ok now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 03:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6q-fec-dump/m-p/679742#M104952</guid>
      <dc:creator>Jacky_Song</dc:creator>
      <dc:date>2017-06-12T03:04:48Z</dc:date>
    </item>
  </channel>
</rss>