<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Temperature dependent on DDR memory calibration ? Reason for kernel panic when the imx6q system get heat-up ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Temperature-dependent-on-DDR-memory-calibration-Reason-for/m-p/679402#M104889</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;@&lt;A _jive_internal="true" data-content-finding="Community" data-userid="206296" data-username="igorpadykov" href="https://community.nxp.com/people/igorpadykov" style="color: #5e89c1; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;igorpadykov&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thank you for your explanation.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Today I encountered a new problem with my iMX6Q custom hardware design with&amp;nbsp;Linux version 4.1.15-1.0.0_ga+yocto+g76c24a0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an issue with GPU during I&amp;nbsp;launch cameras (System stuck).&lt;/P&gt;&lt;P&gt;Camera launch &amp;gt;&amp;gt; gst-launch-1.0 v4l2src device=/dev/video0 ! autovideosink&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error message &amp;gt;&amp;gt;&amp;nbsp;[galcore]: GPU[0] hang, automatic recovery.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It shows the test patterns without any conflict. When I run&lt;/P&gt;&lt;P&gt;gst-launch-1.0 videotestsrc pattern=0 ! autovideosink&lt;/P&gt;&lt;P&gt;There are no any conflict.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;What can be the cause of this issue ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2017 09:34:44 GMT</pubDate>
    <dc:creator>peteramond</dc:creator>
    <dc:date>2017-07-24T09:34:44Z</dc:date>
    <item>
      <title>Temperature dependent on DDR memory calibration ? Reason for kernel panic when the imx6q system get heat-up ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Temperature-dependent-on-DDR-memory-calibration-Reason-for/m-p/679400#M104887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have done DDR memory calibration for my imx6q custom hardware design in ambient temperature and got proper and reliable read,write,dqs gating values for DDR memory. And I updated u-boot configs according to those values.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when the system get heat up; as an example when the die temperature of the imx6 exceed 55C the system shows kernel panic. It is difficult to identify the reason&amp;nbsp;using the errors pop-up in kernel panic using program counter. (May be this is not a reason in processor because imx6 can work up to 85C without de-clocking)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;STRONG&gt;Do we need to do DDR memory calibration in different temperatures before do the updates in u-boot ? Any dependency on memory calibration on temperature ?&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;How can we get temperature profile using few thermocouples which were placed on different areas of DDR memory chips, imx6 processor and etc by using imx6q libraries ?&lt;/STRONG&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Jul 2017 02:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Temperature-dependent-on-DDR-memory-calibration-Reason-for/m-p/679400#M104887</guid>
      <dc:creator>peteramond</dc:creator>
      <dc:date>2017-07-23T02:43:01Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature dependent on DDR memory calibration ? Reason for kernel panic when the imx6q system get heat-up ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Temperature-dependent-on-DDR-memory-calibration-Reason-for/m-p/679401#M104888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. if heating up the part causes more failures, then the drive strength is too low and the &lt;BR /&gt;signals may not rise/fall fast enough. There is no need to perform DDR memory calibration in &lt;BR /&gt;different temperatures, temperature influence is described in sect.7.2 ZQ Calibration Usage &lt;BR /&gt;AN4467 i.MX6 Series DDR Calibration&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4467.pdf" rel="nofollow" target="_blank"&gt;http://cache.nxp.com/docs/en/application-note/AN4467.pdf&lt;/A&gt;&lt;BR /&gt;2. please refer to AN4579 i.MX 6 Series Thermal Management Guidelines&lt;BR /&gt;&lt;A href="http://cache.nxp.com/docs/en/application-note/AN4579.pdf"&gt;http://cache.nxp.com/docs/en/application-note/AN4579.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Jul 2017 23:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Temperature-dependent-on-DDR-memory-calibration-Reason-for/m-p/679401#M104888</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-07-23T23:05:56Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature dependent on DDR memory calibration ? Reason for kernel panic when the imx6q system get heat-up ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Temperature-dependent-on-DDR-memory-calibration-Reason-for/m-p/679402#M104889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;@&lt;A _jive_internal="true" data-content-finding="Community" data-userid="206296" data-username="igorpadykov" href="https://community.nxp.com/people/igorpadykov" style="color: #5e89c1; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;igorpadykov&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thank you for your explanation.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Today I encountered a new problem with my iMX6Q custom hardware design with&amp;nbsp;Linux version 4.1.15-1.0.0_ga+yocto+g76c24a0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an issue with GPU during I&amp;nbsp;launch cameras (System stuck).&lt;/P&gt;&lt;P&gt;Camera launch &amp;gt;&amp;gt; gst-launch-1.0 v4l2src device=/dev/video0 ! autovideosink&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error message &amp;gt;&amp;gt;&amp;nbsp;[galcore]: GPU[0] hang, automatic recovery.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It shows the test patterns without any conflict. When I run&lt;/P&gt;&lt;P&gt;gst-launch-1.0 videotestsrc pattern=0 ! autovideosink&lt;/P&gt;&lt;P&gt;There are no any conflict.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;What can be the cause of this issue ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 09:34:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Temperature-dependent-on-DDR-memory-calibration-Reason-for/m-p/679402#M104889</guid>
      <dc:creator>peteramond</dc:creator>
      <dc:date>2017-07-24T09:34:44Z</dc:date>
    </item>
  </channel>
</rss>