<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6 DL Custom Board EMI Issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678897#M104813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please help identifying which module operates at this frequency of 220-230 MHz; fundamental or harmonic.&lt;/P&gt;&lt;P&gt;We performed the EMI tests at various stress levels, with and without casing, and the frequency of the spike shifted between 220-230 MHz.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 13 May 2017 05:02:36 GMT</pubDate>
    <dc:creator>sohailakram</dc:creator>
    <dc:date>2017-05-13T05:02:36Z</dc:date>
    <item>
      <title>i.MX6 DL Custom Board EMI Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678895#M104811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="padding: 0px;"&gt;Hi Everyone,&lt;/P&gt;&lt;P style="padding: 0px;"&gt;&lt;/P&gt;&lt;P style="padding: 0px;"&gt;We recently tested our iMX6 DL custom board with DDR3 for EMI and EMC. The board is primarily based on SABRE Platform with PMIC. For layout, we used layer stack-up as defined in SABRE Platform.&amp;nbsp;&lt;/P&gt;&lt;P style="padding: 0px;"&gt;We are experiencing an unwanted spike at 230 MHz that exceeds the FCC Class B specified level. We tested up to 6GHz. Everything is fine in complete range except that 220-230 MHz spike. We are unable to identify this frequency either as fundamental or a harmonic for all clock frequencies used in iMX6 and PMIC.&lt;/P&gt;&lt;P style="padding: 0px;"&gt;The EMI Lab suggested ferrite beads on all power sources. I was wondering if any member of community has experienced&amp;nbsp;anything like this during their EMI testing and what possible solution is there to this kind of problem.&amp;nbsp;&lt;/P&gt;&lt;P style="padding: 0px;"&gt;I'd appreciate your suggestions.&amp;nbsp;&lt;/P&gt;&lt;P style="padding: 0px;"&gt;&lt;/P&gt;&lt;P style="padding: 0px;"&gt;UPDATE: EMI Testing report for our board is attached for reference.&lt;/P&gt;&lt;P style="padding: 0px;"&gt;&lt;/P&gt;&lt;P style="padding: 0px;"&gt;Sohail&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 19:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678895#M104811</guid>
      <dc:creator>sohailakram</dc:creator>
      <dc:date>2017-05-12T19:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 DL Custom Board EMI Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678896#M104812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sohail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6Q Sabre SD board passed EMI test and its lab report can be obtained&lt;/P&gt;&lt;P&gt;creating service request.&lt;/P&gt;&lt;P&gt;How to create service request :&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fdocs%2FDOC-329745" rel="nofollow" target="_blank"&gt;https://community.freescale.com/docs/DOC-329745&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For finding cause of spike one can try to disable peripherals one by one, run test&lt;/P&gt;&lt;P&gt;from iRAM, use system pll spread spectrum, slightly change pll frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 23:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678896#M104812</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-12T23:17:43Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 DL Custom Board EMI Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678897#M104813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please help identifying which module operates at this frequency of 220-230 MHz; fundamental or harmonic.&lt;/P&gt;&lt;P&gt;We performed the EMI tests at various stress levels, with and without casing, and the frequency of the spike shifted between 220-230 MHz.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 May 2017 05:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678897#M104813</guid>
      <dc:creator>sohailakram</dc:creator>
      <dc:date>2017-05-13T05:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 DL Custom Board EMI Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678898#M104814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sohail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid it is impossible to say without testing, please try to gate&lt;/P&gt;&lt;P&gt;module clock and check when harmonic disappears.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 03:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DL-Custom-Board-EMI-Issue/m-p/678898#M104814</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-15T03:43:47Z</dc:date>
    </item>
  </channel>
</rss>