<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Direct Camera Input using HDMI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Direct-Camera-Input-using-HDMI/m-p/196530#M10478</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Grahame,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am very sure this option is not available on the HDMICARD (and the way it is connected to the i.MX53 video output only).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you require a commercial HDMI to CSI (Camera Sensor Interface) solution, there might be converter boards for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Dec 2011 11:20:36 GMT</pubDate>
    <dc:creator>sidebranch</dc:creator>
    <dc:date>2011-12-19T11:20:36Z</dc:date>
    <item>
      <title>Direct Camera Input using HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Direct-Camera-Input-using-HDMI/m-p/196529#M10477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The HDMI standard has connectability for video output and input in its specification.&lt;/P&gt;&lt;P&gt;Thence I ordered the additional MCIMX-HDMICARD board part (24bit HDMI MX535/08) to supplement my MX53 Quick Start EVB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the board vendor has connected these pins and allows user to use them is also a matter of interest.&lt;/P&gt;&lt;P&gt;So, my questions to those knowledgeable on such matters -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I connect and use a digital camera output directly to the HDMI connector (as video input) ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;If so, what functionality is available on-board for such usage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Much thanks.&lt;/P&gt;&lt;P&gt;Grahame&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Dec 2011 02:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Direct-Camera-Input-using-HDMI/m-p/196529#M10477</guid>
      <dc:creator>wildpossum</dc:creator>
      <dc:date>2011-12-17T02:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: Direct Camera Input using HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Direct-Camera-Input-using-HDMI/m-p/196530#M10478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Grahame,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am very sure this option is not available on the HDMICARD (and the way it is connected to the i.MX53 video output only).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you require a commercial HDMI to CSI (Camera Sensor Interface) solution, there might be converter boards for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2011 11:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Direct-Camera-Input-using-HDMI/m-p/196530#M10478</guid>
      <dc:creator>sidebranch</dc:creator>
      <dc:date>2011-12-19T11:20:36Z</dc:date>
    </item>
  </channel>
</rss>