<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックu-boot porting problem from version 2014 to version 2015</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-problem-from-version-2014-to-version-2015/m-p/678536#M104727</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am porting uboot from version 2014-4 to 2015-4 for my custom board.&lt;BR /&gt;I made the changes for uart, booting device etc..&lt;BR /&gt;Since uboot-2014 version works fine, I have copied the mx6q_4x_mt41j128.cfg file from uboot-2014 version to uboot-2015.&lt;BR /&gt;but the booting freezes as shown below:&lt;/P&gt;&lt;P&gt;U-Boot 2015.04-00002-gee628f1769-dirty (May 12 2017 - 14:47:34)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6Q rev1.2 at 792 MHz&lt;BR /&gt;CPU: Temperature 23 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am seeing a lot of code related to ddr in sabresd.c, which was not present in version 2014.&lt;/P&gt;&lt;P&gt;Is there any changes required?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 May 2017 10:50:46 GMT</pubDate>
    <dc:creator>pravverma</dc:creator>
    <dc:date>2017-05-12T10:50:46Z</dc:date>
    <item>
      <title>u-boot porting problem from version 2014 to version 2015</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-problem-from-version-2014-to-version-2015/m-p/678536#M104727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am porting uboot from version 2014-4 to 2015-4 for my custom board.&lt;BR /&gt;I made the changes for uart, booting device etc..&lt;BR /&gt;Since uboot-2014 version works fine, I have copied the mx6q_4x_mt41j128.cfg file from uboot-2014 version to uboot-2015.&lt;BR /&gt;but the booting freezes as shown below:&lt;/P&gt;&lt;P&gt;U-Boot 2015.04-00002-gee628f1769-dirty (May 12 2017 - 14:47:34)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6Q rev1.2 at 792 MHz&lt;BR /&gt;CPU: Temperature 23 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am seeing a lot of code related to ddr in sabresd.c, which was not present in version 2014.&lt;/P&gt;&lt;P&gt;Is there any changes required?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 10:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-problem-from-version-2014-to-version-2015/m-p/678536#M104727</guid>
      <dc:creator>pravverma</dc:creator>
      <dc:date>2017-05-12T10:50:46Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot porting problem from version 2014 to version 2015</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-problem-from-version-2014-to-version-2015/m-p/678537#M104728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found the problem, it was some connection issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now u-boot is booting fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 14:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-problem-from-version-2014-to-version-2015/m-p/678537#M104728</guid>
      <dc:creator>pravverma</dc:creator>
      <dc:date>2017-05-12T14:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot porting problem from version 2014 to version 2015</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-problem-from-version-2014-to-version-2015/m-p/678538#M104729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi praveen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as additional help one can use attached Porting Guide, pay attention&lt;/P&gt;&lt;P&gt;to Chapter 1 Porting U-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 23:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-porting-problem-from-version-2014-to-version-2015/m-p/678538#M104729</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-05-12T23:23:50Z</dc:date>
    </item>
  </channel>
</rss>