<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: android booting failed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-failed/m-p/678167#M104659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bowen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for writing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which Android version are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2017 16:18:51 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2017-06-13T16:18:51Z</dc:date>
    <item>
      <title>android booting failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-failed/m-p/678166#M104658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After downloading images on SD with MFG,I create a file in the data partition,after that,android boot failed.here some logs&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;main log：&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;init: Waiting for /dev/.coldboot_done took 0.44s.&lt;BR /&gt;init: Failed to read from /dev/hw_random: No such device&lt;BR /&gt;init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory&lt;BR /&gt;init: do_start: Service watchdogd not found&lt;BR /&gt;Console: switching to colour dummy device 80x30&lt;BR /&gt;init: Failed to read from /dev/hw_random: No such device&lt;BR /&gt;fs_mgr: Enabling dm-verity for system (mode 2)&lt;BR /&gt;fs_mgr: loading verity table: '1 /dev/block/mmcblk3p5 /dev/block/mmcblk3p5 4096 4096 387072 387072 sha256 d6b152556483f363bf3a8db239696d68d3cf450d8271b2744a7d7b787c87b1c4 aee087a5be3b982978c923f566a94613496b417f2af592639bc80d141e34dfe7 10 restart_on_corruption use_fec_from_device /dev/block/mmcblk3p5 fec_start 390129 fec_blocks 390129 fec_roots 2 ignore_zero_blocks'&lt;BR /&gt;device-mapper: table: 253:0: verity: Invalid number of feature args&lt;BR /&gt;device-mapper: ioctl: error adding target to table&lt;BR /&gt;fs_mgr: Error loading verity table (Invalid argument)&lt;BR /&gt;fs_mgr: Disabling error correction for system&lt;BR /&gt;fs_mgr: loading verity table: '1 /dev/block/mmcblk3p5 /dev/block/mmcblk3p5 4096 4096 387072 387072 sha256 d6b152556483f363bf3a8db239696d68d3cf450d8271b2744a7d7b787c87b1c4 aee087a5be3b982978c923f566a94613496b417f2af592639bc80d141e34dfe7 2 ignore_zero_blocks restart_on_corruption'&lt;BR /&gt;device-mapper: verity: 179:5: data block 0 is corrupted&lt;BR /&gt;reboot: Restarting system with command 'dm-verity device corrupted'&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2015.04 (May 17 2017 - 12:31:21)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6SX rev1.2 at 792 MHz&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Temperature 46 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6SX SABRE SDB&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 1 GiB&lt;BR /&gt;PMIC:&amp;nbsp; PFUZE100 ID=0x11&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No panel detected: default to Hannstar-XGA&lt;BR /&gt;Display: Hannstar-XGA (1024x768)&lt;BR /&gt;Video: 1024x768x18&lt;BR /&gt;gis input --- No input&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337052"&gt;log.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 09:35:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-failed/m-p/678166#M104658</guid>
      <dc:creator>bowenzhang</dc:creator>
      <dc:date>2017-06-07T09:35:24Z</dc:date>
    </item>
    <item>
      <title>Re: android booting failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-failed/m-p/678167#M104659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bowen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for writing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which Android version are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 16:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-failed/m-p/678167#M104659</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2017-06-13T16:18:51Z</dc:date>
    </item>
  </channel>
</rss>