<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mux of cspi on the iMX53 QSB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mux-of-cspi-on-the-iMX53-QSB/m-p/196424#M10463</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes the Daisy Chain was correct. It was the hdmi/display-output on the expander which tries to send data, even when it wasn´t set as IPU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Sep 2012 07:28:41 GMT</pubDate>
    <dc:creator>Stefan1z</dc:creator>
    <dc:date>2012-09-20T07:28:41Z</dc:date>
    <item>
      <title>mux of cspi on the iMX53 QSB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mux-of-cspi-on-the-iMX53-QSB/m-p/196422#M10461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have a i.MX53 QSB and i want to use the CSPI on the expanstion-port. Therefore i muxed the DISP0_DAT0 Pin to CSPI-SCLK, but there is already a signal on it. Even if i muxed it to gpio and set the value, this signal is still present. I controlled the mux with the mxc_iomux_v3_get_pad function from iomux-v3.c and everything seems right.&lt;/P&gt;&lt;P&gt;Is there anything that also uses the DISP0_DAT0 pin i don´t know or i miss?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2012 11:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mux-of-cspi-on-the-iMX53-QSB/m-p/196422#M10461</guid>
      <dc:creator>Stefan1z</dc:creator>
      <dc:date>2012-09-19T11:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: mux of cspi on the iMX53 QSB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mux-of-cspi-on-the-iMX53-QSB/m-p/196423#M10462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefan1z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you configure the Daisy Chain as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CSPI_IPP_CSPI_CLK_IN_SELECT_INPUT = 0b00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-ni.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2012 21:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mux-of-cspi-on-the-iMX53-QSB/m-p/196423#M10462</guid>
      <dc:creator>NicolasIzquierd</dc:creator>
      <dc:date>2012-09-19T21:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: mux of cspi on the iMX53 QSB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mux-of-cspi-on-the-iMX53-QSB/m-p/196424#M10463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes the Daisy Chain was correct. It was the hdmi/display-output on the expander which tries to send data, even when it wasn´t set as IPU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2012 07:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mux-of-cspi-on-the-iMX53-QSB/m-p/196424#M10463</guid>
      <dc:creator>Stefan1z</dc:creator>
      <dc:date>2012-09-20T07:28:41Z</dc:date>
    </item>
  </channel>
</rss>